Njord by Trelleborg is a unique series of polymer solutions engineered with decades of offshore industry insight to provide flexibility, buoyancy and protection solutions to the toughest subsea challenges.
Learn more about how we solve your challenges

Deepwater performance in Brazil
The Petrobras P-58 FPSO, which operates on the Baleia Azul field in the Parque das Baleias area, north of the Campos Basin in Brazil, is moored 48 miles / 78 km offshore in a water depth of 4,593 feet / 1,400 meters, and is expected to last 25 years. Oil production, which commenced in March 2014, comes from 19 satellite wells connected individually to the unit.

A buoyant future for oil & gas exploration in Azerbaijan
Situated in the South Caspian Sea, off the coast of Azerbaijan, the Shah Deniz gas field stands at a depth of 600 meters, covering approximately 860 square kilometers. There is a growing requirement in deepwater applications such as this for flowlines to perform under high temperature and high pressure conditions. Large cyclic changes can cause expansion of the flowline, resulting in lateral or upheaval buckling. At a depth of 600 meters / 1,968 feet below surface, these flowlines will come under significant force.

Bespoke flow assurance in Nigeria
Located roughly 60 miles offshore Nigeria, the Erha North phase two development sits at 3,960 feet / 1,200 meters deep and is an extension of the existing Erha subsea system and infrastructure. The existing system is currently producing to the Erha floating production, storage and offloading (FPSO) vessel

Raising the solution up a level to deliver water to Cyprus
A pioneering engineering project, the Mediterranean Subsea Water Pipeline will see 75 billion cubic metres of fresh water delivered to Northern Cyprus each year from the Mersin province in southern Turkey.
High level performance for world’s first subsea gas compression facility
Located on the Halten Bank in the Norwegian Sea, about 200 km from mid-Norway, Åsgard is a central hub and a significant oil and gas producer. It is also the first field in the world to use seabed gas compression. The decision to adopt this new technology on the Åsgard field is expected to maintain production and an increased recovery equivalent to approximately 278 million in barrels of oil when the project is realized.