Trelleborg Showcases Portfolio of High Performance Tooling Materials at SAMPE Baltimore

SAMPE Baltimore
Trelleborg’s advanced engineering and materials (AEM) operation, leading global manufacturer of high performance tooling materials for aerospace, electronics and industrial markets, will showcase its comprehensive suite of premium epoxy tooling materials as well as adhesives, sealers and pastes at this year’s SAMPE Baltimore.
Trelleborg’s complete range of premium epoxy tooling materials offers customers a selection of low density and ultra-high temperature materials designed for the manufacture of precise and stable master models and molds. These will be on view on stand G57 along with high temperature adhesives and color pastes, as well as the recently launched Sealer, ES930 and Release Agent, ER950.
General Manager within Trelleborg Advanced Engineering and Materials in Boston, Robert Kelly stated: “Trelleborg works hard to continuously innovate and produce solutions that provide performance at every level, meeting stringent customer and industry requirements. Our products are fully tested to give the optimal assurance that they will always perform under high pressure.
“As a result of Trelleborg’s core competencies and unique combination of global manufacturing capabilities and material science, the company has been chosen to provide material solutions for projects in many cutting edge areas, ranging from the deepest oceans to outer space.”
Trelleborg manufactures its range of premium epoxy tooling materials using Eccospheres® made in-house at its factory in Boston, Massachusetts. These thin-walled, hollow glass microspheres are developed to meet demanding strength, weight and electrical specifications for materials used in the aerospace, electronics, and industrial markets. To the naked eye they resemble a fine, white, free-flowing powder; however magnification reveals them to be near perfect spheres. Eccospheres® help reduce costs, enhance specific properties and improve material processing.
In addition to high performance tooling materials, Trelleborg will also showcase its ER950 release agent specially formulated to work across the entire range of its epoxy tooling material portfolio. The easily applied solution offers superior finishing and allows Trelleborg to offer a complete suite of products for tool and mold manufacture.
Trelleborg’s ES930 high gloss mold and tool sealer has been specially formulated to seal all types of substrates. With a low odor and a quick cure, the easily applied solution offers superior sealing capability and can be used with all composite media – pre-pregs, resin transfer mold and infusion processes, allowing customers to purchase a complete suite of products from one manufacturer.
SAMPE Baltimore is the only conference and exhibition exclusively dedicated to advanced materials and processes. This event features a high-quality technical conference which features the latest technologies and research advancements concerning the advanced materials and processes community.
This press release is available for download in English. If you reproduce information from this release please give contact details as:
www.trelleborg.com
E-mail: news@trelleborg.com