Secure supply
Underneath conurbations worldwide, complex networks of pipes supply fresh drinking water and manage wastewater. Trelleborg solutions provide leak-tight infrastructure to ensure water security and protect the environment against discharge of sewerage, while in houses specialist seals that are engineered to stand up to potable water feature in faucets and shower heads.
Digging up and replacing sewer pipes is a messy, time-consuming, and environmentally challenging undertaking. Trelleborg’s trenchless solutions provide minimal disruption to the community, traffic, and environment at an overall lower cost to complete pipe replacement. By lining pipes and sealing them from the inside through existing access chambers, Trelleborg’s no-dig technology, prevents environmental pollution and traffic delays caused by tearing up streets. With “Main to House, MTH”, Trelleborg has also solved the issue of sealing residential lateral pipes from the street, so there is no need to go into property owners’ homes or to rip up their yards to replace pipes.