contactusurl /sv-se/seals/search Inga resultat Animation is not fully supported in Internet Explorer versions item found items found item found sidor av Sök Visar På denna sida Your Browser is outdated Återförsäljare Distributör Official Dealer Premium Partner adresser adresser Articles Regulatoriskt pressmeddelande,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Trelleborg Exhibits Innovations for Off-highway Applications at CONEXPO-CON/AGG

Visit us
Fort Wayne, IN, January 2026 – Trelleborg Sealing Solutions exhibits advanced solutions for heavy equipment at CONEXPO-CON/AGG in Las Vegas, Nevada, US, from March 3 to 7, 2026, at booth S82506.
Michael Cook, Global Segment Director Off-Highway, says: “CONEXPO-CON/AGG is the perfect platform to showcase Trelleborg’s innovative sealing solutions for hydraulics and powertrain applications. We’re excited to connect with industry leaders and demonstrate how our advanced technologies are driving efficiency, durability and sustainability in demanding environments today and into the future.”

Featured at the show are the new Stefa® Cassette seals designed for tractors, construction equipment and heavy-duty vehicles. They integrate multiple sealing lips, a protective metal casing and an internal sleeve to create a robust barrier against contaminants while retaining lubricants. 

Cook notes: “Off-highway equipment faces mud, water and abrasive debris that can destroy conventional seals. Our Stefa® Cassette seals provide robust protection in these environments. By combining advanced sealing technology with durability and ease of installation, we’re helping customers reduce downtime and extend service life.”

On display are Trelleborg’s H2Pro™ range of sealing materials for the next generation of off-highway equipment, including a new ethylene propylene diene monomer (EPDM) rubber for high-pressure hydrogen environments across a wide range of temperatures, and a unique thermoplastic polyurethane (TPU) for very low temperatures.

James Simpson, Global Segment Director Energy, says: “Hydrogen has a major role to play in the transition to a carbon neutral world, both as a fuel source and as a storage medium for surplus energy from renewable sources. Due to its inherent characteristics, hydrogen is difficult to seal. The expanding H2Pro™ range, engineered by our advanced global R&D teams, offers reliable sealing solutions for a wide array of off-highway applications including pumps, valves and connectors.”

Trelleborg also showcases its Stefa® High-Performance Radial Shaft Seals. The portfolio is designed for modern industrial environments characterized by high-volume production, 24/7 manufacturing, rapid machinery movement and the necessity to minimize downtime and cost while maximizing operational efficiency.

Inderjeet Singh, Global Product Line Director Rotary Seals, says: “The Stefa® High-Performance Seals are proven to outperform conventional rotary seals. They provide customers with efficient, durable solutions to the extreme duty cycles, higher speeds and challenging operating conditions of today’s rotary sealing systems used in off-highway equipment.”

Attendees can also learn about Trelleborg’s solutions for hydraulic applications. Cook explains: “Hydraulic systems typically use a complex configuration of high-performance seals. Our product range includes seals and wipers designed for hydraulic cylinders such as the Zurcon® polyurethane U-Cup RU9, O-Ring Energized Zurcon® Glyd Ring D and Zurcon® Scraper DA24.”

On display are Trelleborg’s HMF17 FlatSeal™ flat gasket materials that help prevent leaks in off-highway equipment. They demonstrate high compressibility and excellent adaptability, even at low surface pressures. Their unique composition allows them to flow into the microscopic valleys and voids of a flange or other mating surface, effectively eliminating potential leak paths that traditional gaskets might leave open. This ability to conform ensures a tighter, more durable seal from installation.

Other highlights at the show include Trelleborg’s high-performance thermoplastic solutions, advanced composite materials, mechanical face seals, silicone products and conductive materials. 

Trelleborg will share its latest news, technology advancements and market insights on February 4 at 2:05 pm CST via Zoom during CONEXPO-CON/AGG’s virtual press conference. Executives and subject-matter experts are welcome to attend. RSVP through CONEXPO-CON/AGG by emailing ShowMediaServices@aem.org

Learn more about Trelleborg Sealing Solutions: trelleborg.com/en/seals. For further details about CONEXPO-CON/AGG: conexpoconagg.com 
 

Download

Icon_PR

Press Release