contactusurl /es-es/marine-and-infrastructure/search Sin Resultados Animation is not fully supported in Internet Explorer versions item found items found item found items found de Búsqueda y ayuda Showing ¿Desea más información? Your Browser is outdated Distribuidor Distribuidor Official Dealer Premium Partner direcciones direcciones Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Trelleborg Launches Dynamoor To Improve Safety And Reduce Costs Of Mooring Vessels

Dynamoor_news_thumbnail
Trelleborg’s marine and infrastructure operation has launched DynaMoor, a safety focused dynamic mooring solution that actively maintains constant tension in mooring lines to dampen vessel movements, eliminating the effect that passing ships and long-period waves have on moored vessels. This means DynaMoor can increase port and terminal throughput by allowing operations to continue in a wider range of conditions, while improving safety and reducing operational costs.

DynaMoor actively dampens vessel motion, which increases the range of environmental conditions in which cargo can be transferred, improving throughput. The risk of parted lines and excessive vessel excursion is significantly reduced, protecting people, assets and increasing uptime. It further enhances safety by keeping constant tension in mooring lines, minimizing ‘snap back’ zones, and reduces the overall amount of wharf furniture required, simplifying day-to-day operations. The system speeds up the berthing process and minimizes workload and manual line handling, improving overall efficiency.

 

Richard Hepworth, President of Trelleborg’s marine and infrastructure operation, says: “The marine industry is in a time of transition. With increasing vessel sizes, the stakes grow higher. Since even a small error in docking and mooring can cause significant damage or even cost lives, higher standards must be met. A demanding environment requires that users of mooring systems adapt and innovate to ensure efficient and safe solutions.

 

“Docking and mooring has a critical role to play in optimizing the efficiency of both the berth and the overall port facility. Process refinement is key. A lean mooring philosophy aims to transform berthing strategies and enhance operations. This approach enables greater control of the operational window, optimizes berth utilization, lowers resource and space requirements, and demands less time and infrastructure investment to increase berthing capacity.”

 

DynaMoor combines the functionality of Trelleborg’s class leading Quick Release Hook with constant tension capabilities to pay in and out mooring lines, actively maintaining constant tension in mooring lines. Used with the ship’s mooring lines and winches or able to operate independently, DynaMoor can form part of a complete jetty solution integrated with Trelleborg’s Quick Release Hooks, AutoMoor, Smart Bollards, or be deployed as a separate system. DynaMoor units can be rail mounted for a wide range of mooring configurations and can come with an optional capstan fitted. Added safety interlocks prevent inadvertent or unauthorized release. The system also has the ability to release mooring lines remotely in an emergency and monitors loads in real time.

 

Trelleborg’s DynaMoor solution is SmartPort enabled and so has the ability to connect with other port assets, allowing port operators to analyze asset performance and apply data insights, to improve day-to-day decision making.