Boldan In-House Lining System® at a glance

Image shows pipe sections  with cutaways that display the result of the Boldan-inhouse-lining-system treatment

How does the Boldan In-House Lining System® differ from the other sewer renovation methods?

wo pipes are shown, one is rusty and damaged, and the other is in perfect condition after being treated with the Boldan-inhouse-lining-system
A pipe-circle treated with Boldan-inhouse-lining-system. Cutaways show treatment results.

Rehabilitating the drainage system for a house in less than one week

Besoin d'aide ? 

Remplissez le formulaire et vous serez contacté dans les plus brefs délais.

Page 1 sur 3