decodedHtml

Precisely pumped dosages

Felix Shädler holding a pump housing between his fingers
Handy medical devices make life easier for people with chronic conditions, and automated dosing systems are gradually replacing regular injections of essential medication. Trelleborg cooperated with WACKER to develop a microinjection pump, the very heart of such devices.

People with chronic illnesses need to monitor their bodies. Diabetics check insulin levels and people suffering from Parkinson’s adjust their apomorphine dosage. Incorrect administering of medication can make treatment less effective or even, in the worst cases, be life-threatening. 

 

Some conditions can be managed well with injected drugs. Portable medical devices, such as insulin pens, are especially convenient, enabling the fast and safe injection of liquid medication in everyday situations. The users, however, still need to remember the dosage and timing precisely.

 

Automated dosing systems go one step further. These palm-sized medical devices can be attached directly to the skin with adhesive plasters, for example. Located on the surface in contact with the patient is an extremely fine needle that extends automatically to inject a preprogrammed quantity of medicine without the user having to make a single move. Precise control regulates delivery of as little as a few microliters of active ingredient over a period of minutes, hours or even several days. This improves the quality of life of those affected, granting them more flexibility and making delivery of medication worry-free.

 

The centerpiece of these medical devices is a tiny microinjection pump that reliably delivers precise doses of essential medication. Trelleborg Sealing Solutions was commissioned by one of the world’s leading suppliers of pharmaceutical and medical products to help develop a pump housing made of plastic and silicone. Deep inside this pump a unique, innovative material from the German chemical industry company WACKER, ensures smooth operation.

 

“The pump’s extremely precise dosage of drugs was crucial to the success of the entire device,” says Felix Schädler, Project Manager at Trelleborg Sealing Solutions, who played a key role in the development.

Microinjection pump

 

The delicate microinjection pump consists of a cylindrical hollow body in which a plunger is moved up and down electrically. It draws the drug from a supply vessel and conveys it to the injection needle. The pump housing comes in different versions that can deliver two microliters or ten microliters of liquid medication. With a length of 15 millimeters, the smaller pump is not much bigger than a fingernail.

 

Friction, sealing and the bonding of two different materials in a very tight space posed a challenge to the developers from the start. In addition to wanting a compact design, the customer also attached importance to the lowest possible cost, as the injection pump in the final medical device is a single-use product. 

 

For safety reasons, all the elements of the dosing system that come into contact with the medication or the user, including the injection pump, must be disposed of after use. But other components, like the housing, motor and battery, can be reused. 

 

“Due to the compact dimensions and low tolerances involved, the part could only be manufactured using two-component injection molding with seals made of liquid silicone rubber,” says Schädler.

 

Processing Liquid Silicone Rubber (LSR) is the field of expertise at Trelleborg’s Stein am Rhein site in Switzerland. The site has a comprehensive cleanroom production facility for medical technology applications, where production takes place under strictly controlled and monitored conditions. 

 

Two-component injection molding is increasingly in demand for medical applications. “Self-adhesive LSR grades are available for foodcontact and medical situations, making two-component injection molding possible for these applications,” says Schädler.

 

When Thermoplastic Elastomer (TPE) proved unsuitable for this specific application, Schädler and his team initially turned to SILPURAN®6700 self-adhesive liquid siliconerubber. WACKER has marketed specially developed silicones for medical technology under the SILPURAN  brand for a little over 10 years. “Inthis LSR line for sensitive applications, we use special formulations that can satisfy particularly demanding purity requirements,” says Dr. Ulrich Frenzel, who works in technical marketing at WACKER.

 

The exceptional adhesion to a number of thermoplastic materials makes WACKER’s self-adhesive LSR grades ideal for two-component injection molding.

 

Tests conducted with the medical-device manufacturer and Trelleborg’s elastomer laboratory in Stuttgart, Germany, demonstrated, among other things, that SILPURAN 6700 can withstand long-term storage with the medication. Since the drugs come into direct contact with the seals, interactions of any kind had to be ruled out. When the pump’s functionality was put to the test, however, it turned out that the friction between the plunger and the cylinder surfaces made of  SILPURAN 6700 was too high.

 

Even the slightest over- or underdosage of medication can lead to life-threatening situations for the user; it is therefore essential for the pump to operate smoothly. If friction between the plunger and cylinder were high, more force would have been required for the pumping action, which in turn would necessitate a different drive and thus a larger device overall. Alternatively, the customer could have used lubricants. Those, however, would inevitably come into contact with the drug being delivered and possibly impair or, in  the worst case, contaminate it. For the same reason, the use of oil-bleeding silicones such as those offered by WACKER for automotive applications was ruled out.

 

But WACKER’s materials specialists managed to find a solution that works without oil.

 

”We presented this challenge to WACKER’s material developers and they very quickly came up with some initial ideas for an innovation that might work,” says Schädler. ”A wholly new materials technology was developed and ready for marketing within just one year.”

 

Dr. Florian Liesener from WACKER’s technical marketing says, “We already had liquid silicone rubbers with self-adhesive properties in our portfolio, as well as products with low coefficients of friction, but none for sensitive applications that offer both together. The micropump was thus the perfect opportunity for us to combine both properties in one silicone.” 

 

The resulting LSR needed properties that appear physically incompatible: high adhesion and low sliding friction — in other words, holding on and letting go at the same time. Impossible, one might think. ”Yet WACKER demonstrably solved this chemical conundrum, without any problems,” Schädler says. 

 

The material developed made its public debut under the name SILPURAN 6760/50 in 2016. To this day, it is the only market-ready, self-adhesive, friction-modified liquid silicone rubber with biocompatibility certificates.

 

SILPURAN 6760/50 plays an important and reliable dual function in the compact drugdelivery device. It may be invisible to its users, but it gives them completely new freedoms.

 


 

For more information, please go to: Healthcare

 


This is an article has been reproduced from Trelleborg's T-Time magazine. To download the latest edition, go to: www.trelleborg.com/t-time