Trelleborg signs Agreement in Principle to sell its shares in TrelleborgVibracoustic to Freudenberg
Trelleborg has signed an Agreement in Principle with Freudenberg to sell its shares in TrelleborgVibracoustic to Freudenberg. The proposed transaction represents the conclusion of the communicated plan for Trelleborg’s exit from the joint venture.
The transaction is subject to signing of a final agreement and, thereafter, conditional upon the approval from relevant authorities. The transaction is expected to be completed in the second quarter of 2016 and would be effective as from January 1, 2016.
“TrelleborgVibracoustic has successfully integrated two global leaders within automotive antivibration solutions, and in the process delivered significant synergies, improved its footprint and strengthened its positions over the past years. Throughout this journey we have enjoyed great co-operation with Freudenberg,” says Peter Nilsson, President and CEO of Trelleborg.
The transaction is based on an enterprise value of EUR 1.8 billion for TrelleborgVibracoustic.
Trelleborg will receive a purchase consideration equivalent to an equity value of SEK ~6.8 billion, in addition to the dividend of SEK ~1.4 billion received in December 2015. This corresponds to a total value of SEK ~8.2 billion. Approximately 10 percent of the purchase consideration is subject to TrelleborgVibracoustic’s forecasted sales performance in 2016 and 2017. Consequently, the final consideration may be somewhat higher or lower than the above equity value.
The purchase consideration corresponds to approximately SEK 25 per Trelleborg share, and will result in a capital gain of SEK ~4 billion (approximately SEK 15 per Trelleborg share) of which the full amount will increase Trelleborg’s equity.
“I am certain that TrelleborgVibracoustic will continue to develop as the global market leader in its segment. The purchase consideration we will receive is in line with our expectations and represents a clean exit option. The transaction allows Trelleborg to further focus on its overall strategy aimed at developing leading positions in selected segments,” concludes Peter Nilsson.
TrelleborgVibracoustic is currently undergoing a process to change its name to Vibracoustic.
Telephone conference
Analysts, investors and media are invited to attend a telephone conference at 10:00 a.m. CET on April 7, 2016. Please see the separate invitation for details.