Ahlsell establishes first heating and plumbing supplies operation in Norway | Trelleborg Group

Ahlsell establishes first heating and plumbing supplies operation in Norway

Ahlsell establishes first heating and plumbing supplies operation in Norway Swedish heating, plumbing and electrical supplies wholesaler Ahlsell, a Trelleborg Group business area, has acquired Norwegian heating and plumbing supplies wholesaler Sjölie & Birch. Sjölie & Birch, which is primarily active in the Oslo area, has annual sales of approx. NOK 80 M. The acquisition of Sjölie & Birch signals the establishment of Ahlsell's first heating and plumbing supplies operation in the Norwegian market. Negotiations started this spring and was finalized by the approval by Norwegian authorities. Further information can be obtained from Ahlsell's President, Göran Näsholm, telephone: +46 (0)8 623 71 00 (mobile: +46 (0)708 237100), Trelleborg AB's Senior Vice President- Corporate Communications, Mikael Byström, telephone: +46 (0)410 670 37 (mobile: +46 (0)708 55 21 69), or via the Trelleborg AB Corporate Communications Department: +46 (0)410 670 00. www.trelleborg.com ------------------------------------------------------------ Please visit http://www.bit.se for further information The following files are available for download: http://www.bit.se/bitonline/1999/09/03/19990903BIT00330/bit0001.doc http://www.bit.se/bitonline/1999/09/03/19990903BIT00330/bit0002.pdf