contactusurl /sv-se/seals/search Inga resultat Animation is not fully supported in Internet Explorer versions item found items found item found sidor av Sök Visar På denna sida Your Browser is outdated Återförsäljare Distributör Official Dealer Premium Partner adresser adresser Articles Regulatoriskt pressmeddelande,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml
Rotary Shaft Seals: Turcon® Varilip® PDR seals – PTFE rotary shaft lip seals suitable for high speed and low pressure environments.
Turcon® Varilip® PDR is the optimum solution for high-speed rotating applications. The rotary shaft seals are constructed from one or multiple Turcon® PTFE based sealing elements which are mechanically retained in a precision machined metal body. The metal body acts as a robust static seal against the housing, preventing thermal cycling, while the Turcon® sealing element offers effective sealing performance on the shaft, even at high rotational speeds. Its low friction characteristics enable stick-slip-free running, which reduces temperature generation, permits higher peripheral speeds and lowers power consumption. This results in enhanced productivity and a long service life, while maximizing the time between planned maintenance cycles.