contactusurl /sv-SE/seals/Search Inga resultat Animation is not fully supported in Internet Explorer versions item found items found item found sidor av Sök Visar På denna sida Your Browser is outdated Återförsäljare Distributör Official Dealer Premium Partner adresser adresser Articles Regulatoriskt pressmeddelande,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Trelleborg Showcases Proven Hydrogen Solutions at Hydrogen Expo 2025

Hydrogen Expo
Trelleborg Sealing Solutions showcases solutions and capabilities for the entire hydrogen value chain at Hydrogen Expo 2025, from May 21 to 23 at Piacenzo Expo, Italy, pavilion 1, booth B120/C143.

Trelleborg highlights its expanding H2Pro™ range of 20-plus materials proven for applications in the production, transport and storage, and end-use of hydrogen, including its FlexiBond solution, designed for use in electrolyzers and fuel cells.

 

>>Explore the H2Pro™ range

 

Solutions for the Entire Value Chain

 

Daniel Hauser, Manager Lead Group Hydrogen, says: “Our comprehensive range of more than 20 H2Pro™ materials, proven in our proprietary testing regimes to meet the requirements of real-world hydrogen applications, are now available for customers across the hydrogen value chain.

 

“We will also showcase one of our latest innovations in the H2Pro™ portfolio, FlexiBond. It enables new design possibilities for electrolyzers and fuel cells by combining the capabilities of large frame seals with a high-stability shape, and reduces the level of investment needed for complex injection molding equipment.”

 

>>Watch the H2Pro™ webinar

 

H2Pro™ materials provide optimal sealing solutions in challenging hydrogen environments including high pressures and low temperatures, and are characterized by minimal hydrogen permeation, resistance to rapid gas decompression (RGD) and excellent abrasion and extrusion properties. The materials can be used to create engineered molded parts including frame seals, rubber-to-metal and rubber-to-plastic components.

 

Unsurpassed R&D Provides Customer Assurance

 

At Hydrogen Expo Trelleborg also highlights its industry-leading R&D capabilities, recently enhanced by a new 93 sq meter/1,000 sq feet hydrogen test facility in Fort Wayne, Indiana, US. The development is part of Trelleborg’s strategic goal to be a leader in hydrogen sealing and testing to help customers navigate the challenges of the entire hydrogen value chain.

 

The extended testing capabilities offered in Fort Wayne include hydrogen leak detection, compatibility, dynamic testing and permeation testing, which are all critical criteria for sealing hydrogen. Engineering experts perform tests that replicate worst-case application conditions for rapid gas decompression. In a high-pressure system, hydrogen can be absorbed into a seal and if the pressure is suddenly relieved, gas trapped in the seal can expand, potentially causing the seal to blister and crack as the gas tries to escape. There are also testing capabilities for pressures up to 1,500 bar/15,000 psi and across all temperature ranges from cryogenic to above 180 °C/350 °F, and environmental thermal cycle testing at various pressure profiles.

 

>>Download the H2Pro™ brochure