contactusurl /ja-jp/medical/search 結果なし Animation is not fully supported in Internet Explorer versions item found items found item found items found of Search& Help Showing 以下の分野の関連製品に興味がある方に Your Browser is outdated Dealer Distributor Official Dealer Premium Partner 住所 住所 Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Trelleborg Exhibits Single-Use Solutions for Biopharma Customers at BPI 2025

chromatography_800x450
Trelleborg Medical Solutions exhibits advanced solutions for biopharmaceutical applications at BPI in Hamburg, Germany, May 12 to 15, 2025, at booth 204.

Showcased is Trelleborg’s BioPharmaPro™ portfolio including fully integrated solutions and single-use tubing and custom-molded parts.

 

Florance Veronelli, Sales Manager, LifeScience Solutions, says: “The combination of polymer materials expertise, advanced manufacturing processes, innovative engineering and quality assurance provided through BioPharmaPro™ enables us to provide unsurpassed support to accelerate the business of our biopharmaceutical customers.”

 

Also highlighted are Trelleborg’s advanced BioPharmaPro™ composite materials used for chromatography columns.

 

Mike Urbanski, Strategic Account Manager, LifeScience Solutions, says: “Single-use systems represent the future in biopharmaceutical processing of therapeutic drugs, with significant advantages over traditional reusable stainless-steel systems. Our lightweight, tight-toleranced, non-reactive BioPharmaPro™ advanced composite columns are designed to replace stainless steel or acrylic multi-use columns. Produced with polypropylene thermoplastics, the raw materials can be recycled after use, offering a more sustainable solution.”

 

Biopharmaceutical single-use systems (SUSs) offer an alternative to traditional reusable systems by eliminating the need for extensive cleaning and sterilization processes. These systems simplify operations and reduce the reliance on resources such as water and energy, which are typically required for maintaining reusable systems.

 

Urbanski continues: “Trelleborg’s BioPharmaProTM adds value for customers through our one-stop shop for complete integrated solutions, from simple products to complex assemblies, allowing system suppliers to focus on drug development while outsourcing the hardware manufacturing expertise and consolidating their supply chain.”

 

Also showcased are BioPharmaPro™ liquid silicone rubber (LSR) molded components delivering exceptional adaptability, crafted in a range of geometries from precise micro-sized designs to expansive large-scale configurations. With state-of-the-art in-house tooling and precision-driven process engineering, the company ensures outstanding quality and unmatched accuracy.

 

Trelleborg will also feature BioPharmaPro™ thermoplastic molded components produced with advanced specialist equipment using high-temperature, engineering-grade resins such as polysulfone (PS), polycarbonate (PC), and polyether ether ketone (PEEK), ensuring exceptional precision and durability.

 

For further details about Trelleborg Medical Solutions, visit www.trelleborg.com/en/medical