contactusurl /en/inthegroove/search No Results Animation is not fully supported in Internet Explorer versions item found items found item found items found of Search & Help Showing On this page Your Browser is outdated Dealer Distributor Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Takeoff and Landing

Banner_Takeoff and Landing
Orkot® advanced composite materials have been specified as standard for challenging sealing and bearing applications for decades, owing to theirproven reliability and unique benefits. Recent advances in material technology have extended the capabilities of the material range into new horizons.-By Jan Sklucki

IN SHORT

METAL COMPONENTS, THOUGH STRONG,

ORKOT® IN AEROSPACE

Orkot_in_Aerospace
ENGINES

Pump2

Orkot® C338, Orkot® C406

High-load capability, good friction
characteristics and low conductivity
mean Orkot® can be applied to
several engine components.

HYDRAULICS & ACTUATION

Pump2

Orkot® C380, Orkot® C480

Hydraulic and actuation systems
rely on Orkot® to provide smooth
operation and long life.

 

HYDRAULICS & ACTUATION

Pump2

Orkot® C380, Orkot® C480

Hydraulic and actuation systems
rely on Orkot® to provide smooth
operation and long life.

 

HYDRAULICS & ACTUATION

Pump2

Orkot® C380, Orkot® C480

Hydraulic and actuation systems
rely on Orkot® to provide smooth
operation and long life.

 

INTERIOR COMPONENTS

Pump2

Orkot® C620

Overhead storage, seats and
anywhere that requires grease-free
lubrication can benefit from Orkot®.

STRUCTURES

Pump2

Orkot® C620

Orkot® is lightweight and strong,
making it ideal for structural
components.

 

STRUCTURES

Pump2

Orkot® C620

Orkot® is lightweight and strong,
making it ideal for structural
components.

 

“More and more specifications are now moving away from metallic components, taking advantage of the benefits of modern materials”

SHAUN WALKER

Development and Process Manager at Trelleborg Sealing Solutions

Flying far and wide

“Composites are outperforming metal in applications all across the plane” 

SHAUN WALKER

Development and Process Manager at Trelleborg Sealing Solutions

Landing Gear

Landing Gear
UPPER LINKAGES

Due to the hidden position of the upper
pin, reliability is critical. The small contact
area, combined with high loading, requires
a versatile material, such as Orkot®.

UPPER BEARING

Orkot® offers low static and dynamic
friction with minimal stick-slip for smooth
operation over a 20 year service life.

LOWER BEARING

The high sideloading on lower bearings
mean that Orkot® is the perfect material
to replace standard metallic bearings,
whilst providing other benefits.

LOWER LINKAGES

Linkages, such as those within the
retracting actuator, require smooth
operation. Orkot® minimizes stick-slip,
while reducing static and dynamic friction.

HIGH PERFORMANCE MATERIALS

Orkot-C620

ORKOT® C620

Orkot-C384

ORKOT® C384

Orkot-C338

ORKOT® C338

Orkot-C480

ORKOT® C480

Orkot-C406

ORKOT® C406

Orkot-C380

ORKOT® C380