contactusurl /fr-fr/anti-vibration-solutions/search Votre recherche n\'a donné aucun résultat. Animation is not fully supported in Internet Explorer versions item found items found item found items found de Recherche et aide Showing Recherchez-vous cela ? Your Browser is outdated Revendeur Distributeur Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Knopf
Is Required.
decodedHtml

Mountfinder Pro Anti-vibration mount selection made easy

Mountfinder-Pro-APP-hero-image_002
Trelleborg Antivibration Solutions a développé l'application idéale pour mesurer les vibrations des machines critiques et trouver la bonne pièce pour résoudre les problèmes liés aux vibrations : MountFinder Pro.

Vibration is unavoidable in the industrial space and knowing how to manage it effectively isn’t an easy challenge. It requires not only the most innovative products on the market but also a tool for finding the right components for specific machine applications. With that in mind, Trelleborg’s anti-vibration solutions operation has revamped the MountFinder Pro App.

 

Après des années de tests sur différents types de machines vibrantes pour garantir une précision totale et des capacités améliorées, MountFinder Pro est désormais la seule application de mesure des vibrations et du bruit dont vous avez besoin.

 

Qu'est-ce que l'application MountFinder Pro ?

MountFinder Pro uses a Analyseur de vibrations, noise recorder and mount selection technology to identify the best anti-vibration mount required for a specific application – all from a mobile phone. This newly updated app takes advantage of the accelerometers within mobile devices to directly measure a machine's vibration levels. This is simply done by placing your mobile phone on the tool you’re looking to measure.

 

By inputting information such as the number of mounts and machine weight, the app cross-references with the Trelleborg Solutions antivibratoires product database to quickly identify which anti-vibration mount is right for your application.

 

Once you’ve collected your data with MountFinder Pro, you can then get in touch with a specialist member of the Trelleborg team through the app. From there, you’ll have access to specialist insight and support to enable you to select the right solution for your application and begin your journey to smoother, more efficient machine operation.

 

La technologie

All mobile phones contain accelerometers which can measure movement and its direction – the same technology that knows when to rotate your screen while viewing your phone. MountFinder Pro measures the movement of the internal sensor over a short period of time and uses complex mathematics to convert the information to a frequency measurement.

 

Pour s'assurer que l'application est toujours disponible pour fournir l'assistance dont vous avez besoin, quand et où vous en avez besoin, MountFinder Pro a été développé pour suivre la vitesse incroyable des smartphones actuels. Il a également été conçu pour fonctionner avec les smartphones à venir et rester un outil fiable même après les mises à jour des téléphones.

 

New features

La nouvelle version de l'application dispose désormais d'une base de données de produits beaucoup plus importante qui reflète l'étendue des solutions que Trelleborg peut fournir. Cela signifie également que l'application trouvera le produit exact dont vous avez besoin en fonction de votre budget.

 

A new feature for the rebuilt version of MountFinder Pro is the ability to connect your phone to a Bluetooth sensor. This can be used if you don’t want to damage your mobile device or if the application you’re looking to measure is in a hard-to-reach place. You can contact Trelleborg from within the app to get a Bluetooth sensor sent to you.

Principales caractéristiques de MountFinder Pro

Pour s'assurer que l'application répond aux exigences des today’s industry, there are several new and improved features to look out for.

 

Résultats précis des vibrations

Des tests continus et des comparaisons avec des équipements de référence vérifiés, ainsi que l'utilisation de la technologie la plus récente, signifient que les résultats fournis par MountFinder Pro lors de la mesure des vibrations des machines sont toujours fiables.

 

Enregistrement du bruit

Wherever there’s vibration, there’s also noise. Generated by the essential movement of machinery, it is inescapable, but it can be managed to create safer and more comfortable working environments. As a new feature of MountFinder Pro, noise is now recorded, and findings factored into solution recommendations.

 

Sélection de produits sans risque

With a greater Gamme de produits now available within MountFinder Pro, it’s much easier to find the solution you need to effectively manage vibration. Using live Données sur le produit alongside measurement results, the app will always select the most suitable solution to your challenge. Plus, with expert support available in-app, MountFinder Pro does the hard work for you.

 

Augmentation de l'offre de produits

With operations spanning the globe, Trelleborg’s expertise in vibration management is unrivalled. Now, that expertise and the range of solutions that goes with it, is built into MountFinder Pro. So, whatever Le défi, the app will be your go-to tool to solve it.

 

Différentes options linguistiques

Pour améliorer l'accessibilité, l'application a été développée jusqu'à présent en trois langues, à savoir l'anglais, l'allemand et le chinois.

 

Pourquoi télécharger l'application MountFinder Pro ?

Whether you’re an engineer or site manager, the MountFinder Pro app is easy to use and will quickly get you to the solutions that you need to effectively manage vibration, optimise machine efficiency and create safer, more comfortable working environments.

 

En cas de vibrations excessives, le cycle de vie des machines devient beaucoup plus court, ce qui peut entraîner des temps d'arrêt liés à la réparation et à la maintenance ou un remplacement coûteux de la machine. En trouvant les bons supports avec Trelleborg, vous pouvez mieux protéger l'investissement de la machine en assurant un fonctionnement efficace pendant toute sa durée de vie.

 

But it’s not just machinery that is disrupted by excessive vibration and noise. People working nearby may also experience discomfort, potentially leading to drops in productivity and even safety-related concerns.

 

The MountFinder Pro app is available worldwide on the Apple App Store  , Google Play Store and can also be accessed on your web browser.

 

Mountfinder QR code

Version mobile