contactusurl /en/marine-and-infrastructure/search No Results Animation is not fully supported in Internet Explorer versions item found items found item found items found of Search & Help Showing On this page Your Browser is outdated Dealer Distributor Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Trelleborg Supports Ocean Cleanup

The-Ocean-Cleanup

In-line with its long-standing commitment to helping to ensure a more sustainable future, Trelleborg’s marine and infrastructure operation is supporting The Ocean Cleanup and its bid to rid the world’s oceans of plastic.

 

This has seen Trelleborg supply The Ocean Cleanup with seven of its floating pneumatic fenders. Typically, these types of fenders are used for energy absorption when ships meet at sea. However, in this application the fenders will be part of one of the solutions tested as giant floating buoys that are connected to create a wind area. This functions as a sail, which pulls The Ocean Cleanup’s advanced passive drifting boom system, System 001/B, forward to help retain plastic for longer periods of time. With harsh conditions in the Pacific Ocean and 1,000 miles from shore, industry leading designed floating buoys are a key factor for this testing period. Trelleborg delivered the fenders via its fender rental service in the Netherlands.

 

The fenders are intended to increase wind current to allow the system to retain plastic for longer periods of time. In June 2019, System 001/B will head back to the Great Pacific Garbage Patch – the largest accumulation zone of plastic in the world, located between Hawaii and California.

 

Richard Hepworth, President at Trelleborg’s marine and infrastructure operation, says: “As a socially responsible company, Trelleborg is committed to help facilitate a more sustainable future for our planet by addressing the problems caused by excessive plastic waste.

 

“So much so, we’re fully invested in Trelleborg Group’s ‘Message in a Bottle’ campaign, which aims to eliminate the single use of plastic bottles across every business within Trelleborg by 2020. Therefore we are delighted to have the opportunity to support The Ocean Cleanup and its goal of turning the tide on marine pollution by removing plastic from our oceans.”

 

The Ocean Cleanup’s System 001/B consists of a 150-meter-long floater that sits at the surface of the water and a tapered three meter deep skirt attached below. The floater provides buoyancy to the system and prevents plastic from flowing over it, while the skirt stops debris from escaping underneath. As the system moves through the water, the plastic collects within the boundaries of the U-shaped system. The concentrated plastic will be brought to shore for recycling and made into durable products. Revenue gained will help fund the clean-up expansion to the remaining four ocean gyres, which are large systems of rotating currents.

 

Trelleborg’s Pneumatic Fenders are ideal for permanent and semi-permanent port applications and for offshore ship-to-ship transfers. Fast and easy to deploy, Trelleborg’s ISO 17357-1:2014 quality assured fenders ensure large clearances are maintained between the hull and jetty or other vessels. Risk of damage during mooring is minimized, protecting people and cargo.

For more information on The Ocean Cleanup, visit: https://www.theoceancleanup.com/