Trelleborg Wins Contract for Johan Sverdrup Oil Field

Trelleborg

Trelleborg Wins Contract for Johan Sverdrup Oil Field

Trelleborg’s engineered products operation announces it has been awarded a contract for the supply of elastomeric bearings to Statoil’s Johan Sverdrup oil field, Norway's largest offshore development in the past three decades.

Located on the Utsira Height in the North Sea, 160 kilometers west of Stavanger, the Johan Sverdup oil field will be operated by electrical power generated onshore, significantly reducing offshore emissions of climate gases. Daily production during the project’s first phase is estimated at 440,000 barrels per day, while peak production is estimated to reach 660,000 barrels daily - 25% of all Norwegian petroleum production. 

The riser platform – the largest of the four platforms comprising the project’s field center – will be the first of the Johan Sverdrup topside to be installed in 2018. Trelleborg will manufacture and deliver 96 custom designed, sliding elastomeric bearings for use across the 23,000 ton platform’s six support points that will be in direct contact with the heavy transport vessel that will deliver the topside, which is being manufactured in South Korea, to the field. 

JP Chia, Engineering Manager for Trelleborg’s engineered products operation, says: “The Johan Sverdrup oil field is one of the largest ongoing projects in the North Sea. Therefore, it is vital that the finest quality bearings were used to successfully secure each of the platform’s support points. We design and manufacture all of our elastomeric bearings specifically for their application, to ensure that they always perform exactly as required. We are very proud to have been selected to supply a project that will be of major importance to Norway for decades to come.”

Trelleborg’s elastomeric bearings are steel plate laminated and installed between the hull of the facility and its modules. They accommodate axial, shear and rotational movement to keep the modules safe from impact, damage and deformation. Similarly, they prevent the concentration of excessive strains and stresses around the mounting points of the modules and the hull caused by adverse sea and weather conditions. 

All of Trelleborg’s bearings are tested to the highest of standards. Trelleborg’s engineering team check the design for specified loads and deformations and the fatigue performance by means of crack growth analysis calculations. After production they are a 100% individually tested at the company’s laboratory for full-scale research and development. The press used for the tests is the largest in the world of its type, with a load capacity of 18,300 metric tons and weighing in at 600 tons. 




For more information, please go to:
www.trelleborg.com/engineered-products 
 

Press Service:
This press release is available for download in English. If you reproduce information from this release please give contact details as:
www.trelleborg.com
E-mail: news@trelleborg.com