The foundation for safe, reliable immersed tunnels
Immersed tunnels play a vital role in modern transport networks, where long-term reliability has an impact on safety, connectivity, and economic resilience. Effective watertight sealing is critical to protect tunnel structures from water ingress, progressive deterioration, and unplanned disruption, all of which can compromise safety and significantly increase lifecycle costs. Through a lifecycle-focused approach, Trelleborg helps tunnel owners and contractors manage structural movement and extreme environmental conditions, enabling immersed tunnels to operate safely, reliably, and sustainably for generations.
Our core capabilities
What we do: Securing long-term watertight performance
We Design
Global engineering expertise to support reliable performance from the start
We Manufacture
In-house, state-of-the-art manufacturing for consistent quality at global scale
We Test
Proven performance through rigorous testing before delivery and on the field
We Inspect
Assessment of existing tunnels with clear recommendations to maintain watertight integrity.
We Service
Experienced on-site support to ensure long-term watertight performance
We Validate
Documented, verified work to provide peace of mind and traceability.
Proven across critical tunnel applications

Immersion Joints
Immersion joints form the critical interfaces between immersed tunnel elements and are required to maintain long-term watertight performance. This is delivered through a combined Gina gasket and Omega seal system, installed using controlled precision clamping.

Segment Joints
Segment joints connect tunnel segments and must accommodate movement while remaining watertight over the long term. This is achieved using Waterstops, Calamity gaskets, and high-performance ACME and VA seals, designed to withstand pressure and structural movement.

Bulkhead Seals
Bulkhead seals temporarily prevent water ingress into tunnel elements during immersion. Once immersion joints are activated, the seals are removed together with the bulkhead panels and reused.

Closure Joints
Closure joints seal the interface between the final immersed tunnel element and the completed tunnel structure. This is achieved using specifically engineered primary and secondary seals to ensure long-term watertight integrity.

Pin & Catch System
Within temporary works for immersed tunnels, Trelleborg delivers engineered polymer solutions to support safe installation, including rubber mantles for pin and catch systems that absorb impact and dampen vibrations—protecting concrete segments and seals during connection and locking.
Global references