contactusurl /fr-fr/anti-vibration-solutions/search Votre recherche n\'a donné aucun résultat. Animation is not fully supported in Internet Explorer versions item found items found item found items found de Recherche et aide Showing Recherchez-vous cela ? Your Browser is outdated Revendeur Distributeur Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Knopf
Is Required.
decodedHtml

Trelleborg AVS reaches new heights

Trelleborg AVS reaches new heights

Trelleborg Solutions antivibratoires atteint de nouveaux sommets dans le secteur de l'aviation. Le site de Leicester a obtenu la certification du système de gestion de la qualité selon la norme AS/EN 9100.

 

AS/EN 9100 is the internationally recognized Quality Management System (QMS) standard, for the aerospace industry. The standard provides a comprehensive quality system for providing safe and reliable Produits to the aerospace industry and also addresses civil & military aviation requirements. AS9100 is based upon ISO9001 and is an essential pre-requisite of achieving supplying to the aerospace sector. La norme AS/EN9100 reprend l'intégralité de la version actuelle de la norme ISO 9001:2015, tout en y ajoutant des exigences relatives à la qualité et à la sécurité.

 

Les principaux fabricants et fournisseurs de l'industrie aérospatiale du monde entier exigent la conformité et/ou l'enregistrement à la norme AS/EN 9100 pour pouvoir faire affaire avec eux. “This accreditation is a significant achievement for Trelleborg Solutions antivibratoires and confirms our position as a trusted supplier to the aerospace industry,” says Max Billinger, BU President.

 

“We’ve long been committed to developing safe components for use across various industries, and as part of this new accreditation we’ll now be keeping pace with industry shifts to remain compliant with this important standard.” Mark Badge, Quality Manager, added: “Our employees in Leicester have worked hard over the last four years to construct the foundation for this achievement, transitioning to 9001:2015 and 14001:2015, and the latest rail standards so this really is a testament to their commitment.”

 

As an aerospace quality Management System (QMS) standard based on ISO 9001:2015, AS9100 Rev D contains additional requirements specific to the aerospace industry. By integrating QMS requirements into a company’s business processes, the Standard makes it possible to identify manufacturers which produce high-quality goods for the aerospace sector, both efficiently and consistently.

Contactez notre équipe Aérospatiale

Demander à un expert