contactusurl /en/inthegroove/Search No Results Animation is not fully supported in Internet Explorer versions item found items found item found items found of Search & Help Showing On this page Your Browser is outdated Dealer Distributor Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

A Change Of Mind

A Change Of Mind
In the debate surrounding eMobility, many objections raised by the media and owners of conventional cars miss the real point. Their arguments are not based on facts and figures, but merely serve as an excuse not to change from the status quo. - By Axel Weimann

IN SHORT

THEY SAY THE EMOBILITY REVOLUTION

Hot-Spot
HiSpin® HS 40
• Flexible for use in a wide temperature range from -45 °C to +200 °C with XLT FKM material
• Seal at top speeds of over 40m/s
HiSpin® PDR RT
• Flexible for use in a wide temperature range from -200 °C to +260 °C with Turcon® materials
• Seals at top speeds of over 60m/s
• Shaft grounding with conductive PTFE
• Minimum frictional torque
Housing seal
• Automated assembly due to form stability
• Flexible design
• Large selection of materials
• Suitable for oil- and waterbased coolants
• Elastomer or multicomponent solutions
Rubore® Radial Damper
• Damping of vibrations above 300Hz
• Designed to meet application requirements
• Large selection of materials

Behavioral change is required

ENABLING ELECTRIC VEHICLE DEVELOPMENT

Axel
AXEL WEIMANN
“So, why not begin changing your mindset now, as electric vehicles are the inevitable future. Don’t look at the negatives, embrace the positives.”

AXEL WEIMANN,
Director Global Segment Automotive, Trucks & Transportation at Trelleborg Sealing Solutions

Car
Change your mindset