contactusurl /en/applied-technologies/search No Results Animation is not fully supported in Internet Explorer versions item found items found item found items found of Search & Help Showing On this page Your Browser is outdated Dealer Distributor Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Trelleborg Launches New Range of Castable Thermoforming Plug Assist Materials

Syntac PR 2020
Trelleborg’s applied technologies operation is launching a range of castable Syntac® thermoforming plug assist materials for manufacturing of thermoformed food, beverage, and pharmaceutical packaging. The Syntac® range of materials are designed specifically for fabrication of plugs and other associated tooling used in thermoforming manufacturing, where the plastic substrate is molded over the plug using pressure forming, to create a thin-gauged thermoformed usable end product.

Syntac® CIS (Core Industrial Solutions), Syntac® HTS (High Temperature Solutions) and Syntac® STS (Strong Tough Solutions) offer high performance, high quality solutions that are easier to machine and faster to hot-swap than alternative materials. By casting the plugs instead of machining, customers can reduce the amount of wasted material and save time by removing the need for CNC-machining or outsourcing for those customers without access to in-house CNC-machining. 

Kerry Lyons, Business Development Manager for Trelleborg’s applied technologies operation in Rochdale, England, states: “Our Syntac® range of materials have been specifically developed to meet the changing needs of our customers. They are available off the shelf with shorter lead-times than previously offered, with manufacturing taking place in our UK facility. Downtime is a real issue for manufacturers, by helping customers to select the right material, they can increase efficiency and improve productivity.”

Syntac® plug assist materials are available as cast, sheet, or bar systems, requiring no specialized tools to machine or finish. Suitable for use up +220 OC, the new Syntac® materials offer improved material distribution, enhanced clarity, and consistent, reliable repeatability. Customer specific inserts can be pre-fitted by Trelleborg to provide a hot-swappable component option, supporting the easy attachment of the plugs to either the ceiling or bed plate of the manufacturing equipment. 

Lyons, continues: “As part of the development process, our new Syntac® materials have been engineered to be lightweight, durable and tough, offering a cost-effective alternative solution to traditional materials. Trelleborg’s applied technologies operation in Rochdale is able to offer additional value-added services to our customers including cast to shape and CNC machining options to further support our customers.”

Trelleborg’s Syntac® CIS and Syntac® HTS materials are made from high-grade epoxy resin and hollow glass microspheres (HGMS), with Syntac® STS made from a novel thermoset polymer matrix. 

Thermoformed packaging such as drinking cups, food containers and pharmaceutical packaging are formed using plug assisted pressure forming. Syntac® plug assist materials are designed to require minimal finishing with an A-class surface finish, resulting in greater repeatability, optimized material distribution and increased plug life.