contactusurl /en/Search No Results Animation is not fully supported in Internet Explorer versions item found items found item found items found of Search & Help Showing On this page Your Browser is outdated Dealer Distributor Official Dealer Premium Partner address addresses Articles Regulatory Press Release,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Easy round the bend

oresundsbron
When train manufacturer Bombardier worked with Trelleborg to make a new version of Trelleborg’s axle guide HALL, they developed something that saved even more energy and maintenance costs.

The innovative HALL® railway hydraulic axle guide unit allows axles to relax a bit into curves while ensuring they remain rigid when running at high speed on a straight track. With HALL, trains run more cost effectively, consume less fuel, emit lower CO2 levels, produce minimal noise as they go through tight curves, and reduce track and wheel maintenance. Unfortunately, Bombardier, one of the world’s leading train manufacturers could not benefit from the HALL technology as it was incompatible with its bogies. 

 

Andreas Wolf, then Chief Suspension Engineer with Bombardier, now Team Manager Engineering Railway within Trelleborg Industrial Solutions, remembers: “Bombardier approached Trelleborg to start a joint development project.” The cooperation produced a special HALL that fits Bombardier trains and extended the design to further improve performance. 

 

In the Bombardier application, the unit must deal with high vertical loads, but essentially the FLEXX® Curve Standard, as it’s called, applies the HALL principle. And it can be retrofitted to Bombardier trains with FLEXX Compact bogies. 

 

The real innovation is the cross-coupled version, where the HALLs on both wheels of an axle are hydraulically connected in what Alexander Zahnbrecher, Business Development Managerwith Trelleborg, describes as a “hydraulic seesaw — when the forces on each wheel are about equal, the system is balanced and rigid, but when they are subject to different forces, the system moves in that direction.” That is particularly useful in starting and stopping or going through tighter curves: Bombardier will be applying it to all new trains running routes with many curves, saving an estimated 145 tons of CO2 in 10 years for every four-car train.  

 

A third version, called Passive Radial Steering, features an intelligent valve that blocks hydraulic movement under certain circumstances and improves performance on even tighter curves. On a 300-meter-radius curve, wheel wear will be reduced by 90 percent. That will come into its own on mountain routes such as in Switzerland, especially since track charges in the country are lower for trains that do less damage to the track.

 



For more information
, please go to:
Antivibration Solutions