Serving the drilling and downhole market for well over forty years, Trelleborg Offshore has an extensive range of reliable, cutting-edge polymer engineered products and solutions.
The drill riser provides a conduit for the drill string and drilling fluids from the ocean floor to the rig. This has significant weight which must be supported by its own structure and ultimately by the drilling vessel. In order to reduce this weight in water to a more manageable amount, discrete buoyancy units are fitted along the length of the riser.
Riser accessories are designed to complement the rigid Drill Riser Buoyancy Modules (DRBMs) so that there is a comprehensive level of support while ensuring a seamless installation of the riser system.
Riser Protection, protects people, structures and equipment from all types of fire and corrosion in the offshore environment, as well protecting the riser itself. In the demanding environment offshore it is paramount to ensuring on-board safety.
Crushable Foam Wrap is designed to be installed around the inner drill casing which is then immersed within the annulus fluid. As the pressure of the annulus fluid increases, the Crushable Foam Wrap will collapse at a pre-determined pressure/temperature combination, allowing expansion of the annulus fluid and dispersing any potentially destructive pressure increases
Address:Stanley Way, Skelmersdale, Lancashire, WN8 8EA
Phone: +44 1695 712 000
Address: 24 Teed Drive, Randolph, MA 02368
Phone: +1 774 719 1400
Address: 1902 Rankin Rd, Houston, TX 77073, USA
Phone: +1 832 456 8300
Address: Kalosjegata 15, 3055 Krokstadelva, Norway
Phone: +47 32 23 20 00
Address: Rua dos Flutuadores 120, Cabiunas Macaè, RJ, CEP 27970-020 Brasil
Phone:+55 22 2106 4040
Address: Eagle Way, Off Queensway, Rochdale, Lancashire, OL11 1TQ, UK
Phone: +44(0) 1706 716610
Address: Trinity Park, Randall Way, Retford, DN22 7AX
Phone: +44 (0) 1777 712500