contactusurl /sv-se/seals-and-profiles/search Inga resultat Animation is not fully supported in Internet Explorer versions item found items found item found sidor av Sök Visar På denna sida Your Browser is outdated Återförsäljare Distributör Official Dealer Premium Partner adresser adresser Articles Regulatoriskt pressmeddelande,Regulatory press releases only EG. Food Hoses conformity evolution Webinar Selector Button
Is Required.
decodedHtml

Fire and Flame Resistant Rubber Conveyor Belts: A Safety Essential in Material Handling

Fire and flame resistant conveyor belt

In industries where the risk of fire is a constant concern, fire- and flame-resistant rubber conveyor belts play a crucial role in ensuring safety and efficiency. These specialized belts are designed to withstand extreme conditions, providing a reliable solution for transporting materials in environments where flammability is a risk.

What Are Fire- and Flame-Resistant Rubber Conveyor Belts?

Fire and flame-resistant rubber conveyor belts are engineered to resist ignition and limit the spread of flames. Made from materials that are less likely to catch fire, these belts are infused with flame-retardant chemicals that enhance their resistance to high temperatures and sparks. This makes them an ideal choice for industries such as mining, steel manufacturing, and power generation, where conveyor belts are often exposed to intense heat and hazardous conditions.

Fire and flame resistant conveyor belt
Key Features and Benefits
  1. Enhanced Safety: The primary benefit of fire- and flame-resistant conveyor belts is the significant reduction in fire hazards. In the event of a fire, these belts do not contribute to the spread of flames, thereby minimizing damage and protecting workers.
  2. Durability: These belts are designed to withstand harsh environments, including high temperatures, abrasive materials, and heavy loads. This durability ensures a longer lifespan, reducing the need for frequent replacements and maintenance.
  3. Compliance with Safety Standards: Fire- and flame-resistant conveyor belts often meet or exceed industry-specific safety standards, such as those set by the Mine Safety and Health Administration (MSHA), Fire Resistant and Anti-Static standard and the International Organization for Standardization (ISO). Compliance with these standards is crucial for ensuring workplace safety and avoiding regulatory penalties.
  4. Versatility: Available in various grades and configurations, these belts can be tailored to specific applications, from underground mining to bulk material handling in power plants.

Applications

These conveyor belts are widely used in industries where fire safety is paramount. In mining, they transport raw materials through tunnels and other confined spaces where the risk of fire is heightened. In steel manufacturing, they handle hot, heavy materials that can easily ignite conventional belts. Power plants also rely on these belts to transport coal and other combustible materials, ensuring continuous operation without the risk of fire.

 

How does Trelleborg ensure high quality Fire and Flame resistant belts?

Fire and flame resistant conveyor belt

With over 75 years of experience, Trelleborg has established itself as a premium supplier of high-quality rubber conveyor belts. Our specialty lies in producing belts designed for extreme, demanding applications in harsh conditions. Backed by one of the most specialized and well-equipped laboratories, an in-house mixing facility, a robust corporate Trelleborg purchasing network, and a long-standing tradition of expertise in rubber conveyor belt manufacturing, we ensure the highest quality through rigorous control in all manufacturing and development phases. All our fire- and flame-resistant belts are engineered to meet or exceed industry standards, providing our customers with durable, sustainable solutions that deliver the utmost satisfaction.

Summary

Fire and flame-resistant rubber conveyor belts are an essential component of safe and efficient material handling in high-risk industries. By reducing the potential for fire-related incidents, these belts protect both workers and valuable assets, ensuring that operations can continue smoothly even in challenging conditions. Investing in these specialized belts is not just a matter of compliance, but a commitment to safety and sustainability in industrial operations.

For further information contact: 

Rok Šilc

Rok Šilc

Sales Manager
Tel: +386 41 323 843