Trelleborg new Axcyl Carbon Bridge Sleeve | Trelleborg Printing Solutions

Trelleborg new Axcyl Carbon Bridge Sleeve

We are pleased to announce the release of a new Axcyl® Carbon Fiber Bridge aimed at accelerating customers’ performance

The unique construction of the new Axcyl® Carbon BS bridge from Trelleborg, provides exceptional stiffness in flexion, and combined with its innovative damping mounting layer, allows more efficient printing of the most difficult designs on the highest productivity presses, with no offset of printing speeds. It can easily be mounted via an air cushion on the press shaft, onto which plate mounting sleeves can then be mounted via direct air supply or separate ventilation.

Through design engineering, the bridge has been made lighter than conventional composite bridges. In addition, the Carbon BS can be also used on existing presses, to maximize the productivity of installed assets. This product is another step in helping secure our customers’ improved performance.

For more info visit now: New Axcyl Carbon BS bridge sleeve allows more effective printing

trelleborg AXCYLCARBON