Trelleborg Showcases High-Performance Printing Solutions at FESPA

Trelleborg

Trelleborg Showcases High-Performance Printing Solutions at FESPA

Trelleborg will showcase its range of high performance commercial, packaging and screen printing solutions at FESPA Global Print Expo, held in the Messe Berlin, Germany, 15-18 May 2018 on stand 4.1-D13.

On stand, show attendees will get a first-hand look at the companies printing blankets for offset printing including Vulcan Folio, Vulcan Mytho and Vulcan Zenith used in commercial printing, Vulcan Pack UV used in packaging printing, and Vulcan Sunrise for UV applications. In addition, the company will be showcasing its complete range of squeegees consisting of Unitex® Ulon HP and Unitex® Marathon, which covers the full breadth of screen printing applications including printed electronics, graphics, textiles, glass, optical media, bottles and containers. 

Alessandra Bungaro, Communications Manager at Trelleborg’s printing solutions operation states: “At Trelleborg we have fifty years of experience of offset blankets and their impact on press performance. We will have samples of our Vulcan Mytho, the only rubber, neutral-feed, for heat-set applications and Vulcan Folio, the well-known blanket for sheet-fed presses. Both solutions have a history of being successfully used for printing a huge range of products, from books and catalogues to commercial leaflets and magazines.

“We look forward to showcasing our range of unique customer solutions for offset printing applications, from the historical blankets as such Vulcan Mytho and Vulcan Folio to the recently introduced Vulcan Sunrise, the innovative solutions when low energy inks are used”

Paul White, Marketing and Business Development Manager at Trelleborg’s applied technologies operation in Retford states: “We are especially excited to be exhibiting this year as we will be celebrating our 60-year anniversary of manufacturing products made of Vulkollan®, which is a high performing elastomer polyurethane material used in our Unitex® squeegee range.

“We have exhibited at FESPA for many years as it provides a fantastic platform to demonstrate to attendees how our Unitex® range can improve screen printing processes by providing excellent print quality and accuracy, decreasing setup times and extending print runs and prolonging squeegee life.”

Vulcan Sunrise is a 1.96 mm blanket with a dedicated top compound and is specifically designed by Trelleborg for UV applications such as LE/HUV and LED UV. Providing all of the benefits of the Dynatech System e.g. excellent smash and edge mark resistance plus good vibration absorption, Vulcan Sunrise enables first class solids and halftone reproduction. The blanket is suitable for use with direct-drive presses as the Dynatech carcass ensures even power consumption in the drives.

Unitex® screen printing squeegee are available in a wide range of hardness levels, compounds, shapes and profiles worldwide, through our experienced sales team and distributor partners. For additional information regarding the Trelleborg squeegee range click here.

About FESPA Global Print Expo

FESPA Global Print Expo is Europe’s largest exhibition for the wide format print industry.

At the show over 600 exhibitors showcase their latest innovations and product launches in the digital and screen printing sectors for graphics, signage, décor, packaging, industrial and textile applications.

Visit US:

Stand 4.1-D13

FESPA Global Print Expo

May 15-18, 2018

Messe Berlin, Germany,

Email to: printingsm@trelleborg.com

For additional information visit: https://www.fespaglobalprintexpo.com/welcome

Download the entire press release