Trelleborg Exhibits Innovations in Medical Device Components at MD&M West

Medical Device Component
Trelleborg’s Healthcare & Medical experts will be at MD&M West in Anaheim, California, in Hall D, Booth 2601, August 10 to 12, 2021, to exhibit advanced polymer solutions for healthcare and medical applications.

New capability

 

At the show, Trelleborg will announce its latest capability to help healthcare and medical customers expedite their new product development process. This new offering will help minimize production costs, quicken development time, and ensure superior-quality products.

 

Linda Muroski, President of Trelleborg Global Healthcare & Medical and Marketing Americas, says: “This service will accelerate our customers’ time to market and help them achieve their mission of improving patients’ lives. Using our deep knowledge of polymer materials, excellence in manufacturing, and engineering expertise, this new capability will deliver increased value to our customers.”

 

Extruded tubing

 

Visitors to the booth will also see an extensive selection of Trelleborg’s specialty extruded tubing and hose products. Tubes are available in a full range of sizes and are custom designed with customers to meet their individual application needs.

 

Andrew Gaillard, Global Director of Trelleborg Healthcare & Medical, says: “We engineer novel extrusion solutions for our customers’ specific tube and hosing applications. Examples include multi-lumen, silicone foam extrusions, and kink-resistant tubing for a variety of critical applications such as pacemaker and neuromodulation leads and urological implants. Additionally, Trelleborg’s GeoTransTM technology enables the production of extrusion profiles that can change throughout the length of the extrusion, supporting unique, customer-specific designs.”

 

Molded parts

 

Trelleborg will also showcase its molded parts that are often used in implantable healthcare and medical devices. Utilizing in-house precision tooling and expertise, Trelleborg creates custom silicone and thermoplastic molded parts with tight tolerances, while the need for rapid product development is met with quick turnaround prototypes. Additionally, attendees will be able to see Trelleborg’s advancements in multicomponent and micromolding capabilities.

 

Gaillard says: “One of our most well accepted capabilities is the combination of Liquid Silicone Rubber (LSR) with plastics. Commonly referred to as 2C or 2-shot, multicomponent injection molding allows our LSR experts to employ highly sophisticated tool and process engineering to develop innovative solutions that combine two or more individual materials into one fully bonded, robust component.”

 

Silicone sheeting and drug delivery

 

Finally, attendees at MD&M West will see Trelleborg’s silicone sheeting and drug delivery capabilities. These highlight the continued evolution of technologies enabling the development of novel solutions for patient care.

 

“In recent years, we’ve seen a spike in demand from our customer-partners for devices that incorporate an active pharmaceutical ingredient for targeted delivery of a therapy. Whether challenged with a wound-care application that requires wafer-thin silicone gel films with a drug element incorporated, or an innovative approach to cancer treatment with unique manufacturing challenges, our engineering teams are consistently eager to partner with customers to help solve interesting and complex problems,” concludes Gaillard.

 

For further details regarding Trelleborg’s Healthcare & Medical operations,  go to

 

www.trelleborg.com/healthcare