‘Fab Four’ Best-in-Class FFKM Materials for the Most Critical Semiconductor Sealing Applications

10_PureFab_Web News 800x450
Trelleborg Sealing Solutions launches four best-in-class materials in its Isolast® PureFab™ range specifically engineered for critical semiconductor sealing applications. For OEM’s & Fabs, utilizing these unique perfluoroelastomer (FFKM) formulations will provide an increased product yield and decrease process defects. This will reduce downtime, extend product maintenance cycles, give greater process tool uptime, resulting in a lower total cost of ownership.

With excellent mechanical properties, all the ‘Fab Four’ semiconductor materials demonstrate the highest purity of their kind, without compromising plasma resistance, outgassing, or thermal stability. Individually, the materials are best-in-class for specific characteristics: 

  • Isolast® PureFab™ JPF10 for remote plasma resistance with fully organic formulation
  • Isolast® PureFab™ JPF20 for overall plasma resistance and minimal particulation in harsh environments
  • Isolast® PureFab™ JPF21 for long-term thermal stability and low trace metal contamination
  • Isolast® PureFab™ JPF30 for its market-leading high temperature rating and extreme purity in a translucent material

 

Register for the Webinar

On April 27, at 5:00 pm Japan Standard Time (JST) / 8:00 am Central European Summer Time (CEST) and April 28, at 5 pm CEST / 8 am Pacific Daylight Time (PDT), Trelleborg Sealing Solutions semiconductor experts will be hosting a free-to-attend webinar Isolast® PureFabTM FFKM Seals – Maximize System Uptime of Advanced Semiconductor Processes Now.  Our experts will introduce participants to these new materials and demonstrate the benefits they bring to semiconductor manufacturers.  

 

Developing Materials & Proving Performance


Dr. Murat Gulcur, Semiconductor Materials Development Manager at  Trelleborg Sealing Solutions, says: “Listening to the voice of the customer and addressing the requirements of critical front-end processes, we invested significant R&D resources into the development of the four new cutting-edge Isolast® FFKM materials. The new compounds are market-leading and completely in line with the industry’s needs today and, more importantly, the developing needs of tomorrow. 

“Selecting the correct sealing material for semiconductor applications is particularly important in achieving the optimum balance between extending the life of a seal and the chances of contamination. This is made all the more critical by miniaturization. With the most advanced technology node as small as 5 nanometers (nm) today, and 3 nm on the horizon, purity and cleanliness are paramount.

 

“Proving of the materials’ performance took place over 24 months involving extensive testing, including plasma erosion tests in the most common process gasses; as well as long-term mechanical and purity tests, including trace metal analysis and outgassing. 

 

“Equipped with these test results and competitive benchmarking data, Trelleborg engineers can support our customers’ development teams by precisely specifying the most effective sealing material to match the process chemistry, system location and tool complexity of their demanding semiconductor environments. This support and technical data significantly reduce our customers’ risks when qualifying new materials.” 

 

Isolast® PureFab™ Portfolio


Isolast® PureFab™ JPF10 incorporates unique cure technology to improve plasma resistance of organic materials without using any inorganic fillers. This makes it one of the best performing, fully organic materials on the market, offering extremely low trace metal content and providing long service life, even at high temperatures. 

 
Gulcur continues, “In some highly critical semiconductor processes, the requirements of a sealing material can be even more stringent. For example, when a process node is below 10 nm and an elastomer part is in close proximity to wafers, a specially formulated ultra-pure FFKM translucent material without any filler may be required to maintain volume wafer output.” 
 

To this end, Isolast® PureFab™ JPF30 offers unrivalled elevated temperature performance and sealing integrity compared to other translucent materials in the market. 

Isolast® PureFab™ JPF20 incorporates an advanced nanoparticle filler with a very high surface area, meaning the amount of fillers in the material is significantly lower than competitive compounds, which provides the ultimate plasma resistance, while minimizing particle generation.


Another fully synthetic filler system is used in Isolast® PureFab™ JPF21 to offer outstanding high temperature performance up to +320 °C /+593 °F and minimum particulation upon exposure to fluorine-based plasmas. Due to its excellent compression set properties, the compound is suitable for dynamic applications, including bonded slit valve doors.

 

Problem Solving for the Semiconductor Industry

The new Isolast® PureFab™ materials are especially suited for critical seal locations for  leading-edge semiconductor manufacturing processes, in particular plasma processes, including deposition, etching, ashing and stripping, as well as thermal processes, such as oxidation, diffusion, RTP, ALD and metal CVD. 
 
 
Chris Busby, Product Line Director & Semiconductor Segment Lead for Trelleborg Sealing Solutions, adds: “It’s not just about the product itself. Trelleborg Sealing Solutions is renowned for its design and engineering expertise, earning a reputation as a ‘problem solver’ for the semiconductor industry. Global development is backed by local specialist support, wherever internationally acting semiconductor original equipment manufacturers and Fabs need it.” 
 

Find out more