Trelleborg Features Tracks and Brawler Tires at The Rental Show

Trelleborg Features Tracks and Brawler Tires at The Rental Show

Trelleborg Features Tracks and Brawler Tires at The Rental Show

Visit Trelleborg at Booth 4885 at the American Rental Association's annual convention and trade show for the equipment rental industry

WAKEFIELD, Mass. – February 27, 2017 –  Trelleborg Wheel Systems is showcasing its rubber tracks and Brawler tires at booth 4885 at The Rental Show from February 26 to March 1 at the Orange County Convention Center in Orlando, Florida.  

Jared Steier, OE Aftermarket and Rental Sales Manager for Trelleborg’s industrial and construction tires operation, says: “We’re excited to meet directly with customers in the rental market and show them first-hand the benefits of using Trelleborg tires and tracks on their equipment. Our Brawler solid tires and rubber tracks are field-tested to ensure they provide a maximum up-time for machines and deliver excellent overall value.  Trelleborg is proud to be part of the rapidly growing rental market.”

Designed to perform in extreme environments and rigorously tested, Brawler HPS and HD Skid Steer tires feature a durable cut resistant rubber compound, which eliminates downtime caused by flats and sidewall cuts. 

Trelleborg’s rubber tracks are amongst the most cost-effective tracks available in the market today. For example, with its low-vibration design and advanced rubber compound, the CRT-800 – available for compact track loaders, mini-excavators, dumpers, demolition machines and scissor lifts – outlasts and outperforms other tracks in its class.

For further information go to trelleborg.com/en/wheels

Donwload the entire document of the press release, go to:

"Trelleborg Features Tracks and Brawler Tires at The Rental Show"