Trelleborg to Showcase New Products at National Farm Machinery Show, Kentucky
Extending its offering for self-propelled sprayers, Trelleborg has launched the first size of the TM150 line, developed according to BlueTireTM technology. In line with the Very High Flexion standards, the new size VF 380/90R46 173D is able to carry up to 14,300 lbs at 40 mph.
The ProgressiveTraction™ tire, an innovative concept for agricultural tires, is specifically designed to improve farming efficiency by leveraging a double lug design. Operating on the soil at different times, the double lug progressively releases higher traction where and when required. Trelleborg ProgressiveTractionTM technology will be honored with the prestigious FinOvation Award during the upcoming show.
With more than 850 exhibitors covering 1.2 million square feet of floor space, the National Farm Machinery show is the largest indoor farm show in America.
Trelleborg is committed to continually develop solutions that improve the efficiency, productivity and sustainability of modern farming.
To find out more about the TM150 tire and ProgressiveTraction™ technology visit stand 410G at the National Farm Machinery show.