Trelleborg Will Showcase Cutting-Edge Technology at Farm Progress Show

Trelleborg Will Showcase Cutting-Edge Technology at Farm Progress Show

Trelleborg Will Showcase Cutting-Edge Technology at Farm Progress Show

Trelleborg will present its broad range of agricultural tires at the 63rd Farm Progress Show in Boone, Iowa, from August 30 to September 1, 2016 in booth 1019 in the Northwest Quadrant. Agricultural professionals can expect to see a vast range of Trelleborg tires from row crop tires, to its newest technology within the /60 range, TM1060 VF 710/60R38 ProgressiveTractionTM.
Andrea Masella, Trelleborg Brand Manager, Agricultural and Forestry Tires, North America, says: “The Farm Progress Show has grown to become the largest outdoor farm equipment show in the United States. The three day show gives agricultural professionals an interactive environment to gain insight on new products and technologies available to increase their production and add value to their current operations. We invite you to stop by our booth to find the right cutting-edge tire for your operation.”
Among the tires presented at the Trelleborg booth will be the new TM1060 VF 710/60R38 ProgressiveTractionTM, offering up to 40 percent higher load capacity and overall better performance, while keeping a low profile. The new Trelleborg TM1060 not only replicates but surpasses the performance of /60 Series tires. Unlike many existing solutions on the market, the TM1060 is suitable for use on tractors over 300 horsepower and can be used with narrower rims, enhancing tractor efficiency.
In addition, the booth will include the 750/75R46 TM1000 High Power tire with maximized tread design and the widest footprint on the market, providing optimum pressure distribution and the utmost respect for the soil.

For more information on Trelleborg’s complete range of agricultural tires, visit: www.trelleborg.com/wheels/us

Download the entire PDF document of the press release:

"Trelleborg Will Showcase Cutting-Edge Technology at Farm Progress Show"