Trelleborg Exhibits Rubber Belts for Compressive Shrinking at SHANGHAITEX 2015

Trelleborg-Shanghaitex_1024x575
Trelleborg Exhibits Rubber Belts for Compressive Shrinking at SHANGHAITEX 2015

Trelleborg’s rollers and belts operation will be exhibiting its complete product range to leading textile companies from mainland China and the Far East at SHANGHAITEX 2015, to be held in the Shanghai New International Exhibition Center, from 15 – 18 June, 2015.

Attending for the first time, Trelleborg’s rollers and belts operation will showcase its complete Rollin® range of rubber shrinking belts for use on Sanfor, as well as Comfit and mini compressive units for tapes.

Trelleborg’s Rollin® belts grant optimum shrinkage rates and thanks to their new inner face, provide significant improvement in terms of reliability and durability in operation.

Guillaume Bordais, Sales Manager for rollers and belts, says: “In addition to these benefits, our rubber belts enable use with any fabric, knitted or woven cotton, or man-made fibers. Additional key features include a seamless multi-layer structure and outstanding resistance to mechanical and chemical stress, making our range unique in the market place. 

“As a result our customers can benefit from very high shrinking rates, outstanding fabric surfaces and a long operating life in operation.” 

Trelleborg will also showcase its full offering of rubber coverings solutions for rollers in squeezing, dyeing and finishing applications at SHANGHAITEX to give a complete overview of the company’s offering to the market. On stand, customers will be allowed to touch and see a variety of products, including:

• Rollin® Textractor, the solution for homogenous and consistent squeezing with outstanding chemical wear and aging resistance.

• Rollin® Steamtex, a finishing product designed to be used in a closed atmosphere at high temperatures, up to +110 °C It’s light color avoids the risk of stains on fabrics .

• Rollin® Verotex, a dyeing and finishing solution with excellent chemical resistance to acidic and alkaline textile auxiliary products.

Visit Trelleborg at stand W4K31 to find out more.