Learn more about how we solve your challenges

Material expertise supports unique topside safety and protection requirements
Equinor is an energy company with more than 21,000 employees developing oil, gas, wind and solar energy in more than 30 countries.
In order to serve its customers, a new oil field in the North Sea, 140 kilometers west of Stavanger, Norway, Johan Sverdrup was commissioned to open in late 2019. This would become Norway’s third largest oil field, producing 470,000 barrels of oil per day during phase 1, powered using mainly hydroelectric power.
Johan Sverdrup field is around 200 square kilometers in size. At the peak of production, the field will account for roughly 30% of the total oil production on the Norwegian Continental Shelf. With accommodation for 560 people, the field consist of several platforms all linked by bridges, standing in approximately 110 meters of water, making safety of paramount importance.
In order to serve its customers, a new oil field in the North Sea, 140 kilometers west of Stavanger, Norway, Johan Sverdrup was commissioned to open in late 2019. This would become Norway’s third largest oil field, producing 470,000 barrels of oil per day during phase 1, powered using mainly hydroelectric power.
Johan Sverdrup field is around 200 square kilometers in size. At the peak of production, the field will account for roughly 30% of the total oil production on the Norwegian Continental Shelf. With accommodation for 560 people, the field consist of several platforms all linked by bridges, standing in approximately 110 meters of water, making safety of paramount importance.

Certified safety in the Gulf of Mexico
The offshore industry is constantly innovating and increasing in sophistication, resulting in a need for equipment to be much more reliable, effective and safe. Specifically on offshore facilities, rapid fire spread is a high risk, making fire deluge systems absolutely critical. Unfortunately, there are a significant number of aging platforms and rigs across the globe still using substandard carbon steel systems, which are extremely prone to corrosion.