Trelleborg to exhibit at Kormarine 2021

Trelleborg’s marine and infrastructure operation will showcase its portfolio of world-leading energy transfer systems technology at this year’s Kormarine, which will be hosted as an in-person and virtual hybrid event at the Busan Exhibition & Convention Center in Busan, Korea from October 19-22, 2021.
Representatives from Trelleborg will be on hand to discuss its Ship-Shore Links (SSLs), Universal Safety Links (USLs) and Emergency Shutdown Links (ESLs). These systems offer a reliable way of enabling rapid and controlled shutdown should an emergency situation arise during the transfer of LNG, LPG, oil, chemicals and other hazardous liquids. Together with Trelleborg’s Emergency Shut-Down Systems (ESDSs), the links provide an economical and extremely space efficient solution for the provision of the critical SSL – ESDS link in safety systems.
Visitors will also be able to discover everything they need to know about its TSX5 Torsionmeter which enables the measurement of shaft torque and thrust. The solution employs a full strain gauge bridge - the most accurate method of measuring torque – giving confidence to operators that results obtained are reliable.
For more information about Trelleborg’s portfolio of solutions designed to support the entire LNG value chain, visit stand 1E51 at Kormarine 2021.