Platinum Sponsor Trelleborg to Open the LNG Ship/Shore Interface Conference

Platinum Sponsor Trelleborg to Open the LNG Ship/Shore Interface Conference

Date: 28-29 November 2019 | Venue: London, UK


LNG World Shipping Ship/Shore Interface Conference 2019_thumbnail

Platinum sponsor, Trelleborg’s marine and infrastructure operation, will deliver the welcoming address and exhibit at the LNG Ship/Shore Interface Conference in London, UK (28-29 November).

The two-day conference will bring together Europe’s LNG transportation supply chain to discuss ship and terminal operations at the jetty, offshore and bunker station. At the conference, Dave Pendleton, Managing Director of Trelleborg’s marine and infrastructure operation (UK), will discuss the growth of LNG applications and the need for the driving of an industry that increases asset flexibility and reduces OPEX and CAPEX (10:55 AM, 28 November).

Trelleborg will exhibit its Universal Safety Link (USL), which takes the company’s expertise in large-scale LNG transfer applications, develops it and applies it to provide an optimized solution for the small and mid-scale LNG sectors. In addition to the USL, delegates will also be able to learn about Trelleborg’s Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for over 20 years.

Richard Hepworth, President of Trelleborg’s marine and infrastructure operation, said: “The volume of LNG continues to grow, and so too does the breadth of LNG applications. LNGC, FSRU, FLNG and LNG fueling are all leading to increased demand for LNG. Each of these challenging areas requires assets to be as flexible as possible to optimize their returns in these markets. LNGCs need the ability to call at any LNG terminal to load or discharge a cargo. FSRUs need to be able to dock at any CNG terminal with ease and begin providing power, while an FSU may or may not be moored alongside and then trade as an LNGC if required. LNG Bunker barges need to be capable of calling in at a large-scale terminal to replenish and then service any number of LNG-fueled vessels.

“The LNG Ship/Shore Interface Conference provides the perfect platform for the industry to collectively discuss the many challenges across the LNG industry and the innovative ways in which manufacturers like Trelleborg are tackling them head on.”

For more information on Trelleborg’s range of solutions for the LNG industry, visit Trelleborg at the conference exhibition.