Trelleborg to Present at 2019 LNG Bunkering Summit

Trelleborg to Present at 2019 LNG Bunkering Summit

29-31 January 2019 | Venue: Amsterdam, Netherlands

Now in its 7th year, the LNG Bunkering Summit focuses on the entire supply chain, offering insights into decision making, planning, development, operation, safety and training processes that are driving the LNG Bunkering market forward. This is Europe's fastest growing and largest LNG Bunkering Summit at which the future of the industry is discussed annually amongst infrastructure operators, shipping companies, LNG suppliers and technology providers.

Trelleborg Marine Systems will sponsor the 2019 LNG Bunkering Summit, which will be held in Amsterdam, Netherlands (29-31 January).

At the Summit, Paul Radage, Sales Director at Trelleborg Marine Systems, will provide a detailed look at a real-life case study in LNG bunkering, discussing the challenges met and the lessons learned.

On stand, Trelleborg will exhibit its Universal Safety Link (USL), an innovative product that takes the company’s expertise in large scale LNG transfer applications, develops it and applies it to provide an optimized product for the burgeoning and diverse small and mid-scale LNG sectors. Delegates will also be able to learn about Trelleborg’s Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for over 20 years.

For more information about Trelleborg’s range of solutions for the LNG industry, visit: http://www.trelleborg.com/en/marine-systems/products--solutions--and--services/ship-shore--links 


LNG Bunkering Summit 2019