03.03.2020
Eccofloat® composite foams provide high performance and ultra-low densities by using only the highest specification hollow glass microspheres, called Eccospheres®. These are combined within a rigid, high-strength resin system, overcoming the issue of weight for deep sea exploration.
David Clayton, Sales Director for Trelleborg’s applied technologies operation in Europe, states: “Our latest TG11500 material was specifically developed for repeated use in ultra-deep high-pressure environments and specially chosen for the ‘Full Ocean Depth (FOD) Triton’ submersible, which made up a sizeable proportion of the overall body of the manned submersible vessel. Manufactured from full ocean depth material, the TG11500 is a low-density high-performance solution to a unique application.”
On Stand Solutions at Oceanology will include:
Njord Trimsyn syntactic floats designed to offer additional buoyancy in all marine applications and Njord Trimlok umbilical clamping system, created to streamline the attachment of Njord Trimsyn floats.
Njord UB (Umbilical Buoyancy) is designed for use in conjunction with ROVs to keep the required length of umbilical buoyant underwater, constructed using a polyethylene outer shell filled with a high-performance syntactic foam core.
Njord Linksyn & Njord Linksyn HD – Developed to provide buoyancy and bend control to the umbilical on larger trenching vehicles, preventing the umbilical from bending below its minimum bend radius.
Delegates will have the opportunity to meet with Trelleborg composite experts to discuss the importance of selecting the right materials for projects, as well as Trelleborg’s proven manufacturing techniques and in-house CNC capabilities.
About Oceanology International
Oceanology International is the world’s largest ocean technology exhibition and conference, with over 500 exhibitors bringing together businesses, academics and government. The exhibition includes live demonstrations and interactive seminars with over 8,000 attendees across the three days.