12.12.2018
Trelleborg Antivibration Solutions soar to new heights in the Aviation Sector, the Leicester site has achieved Quality Management System certification to AS/EN 9100.
AS/EN 9100 is the internationally recognized Quality Management System (QMS) standard, for the aerospace industry. The standard provides a comprehensive quality system for providing safe and reliable products to the aerospace industry and also addresses civil & military aviation requirements. AS9100 is based upon ISO9001 and is an essential pre-requisite of achieving supplying to the aerospace sector.
AS/EN9100 fully incorporates the entirety of the current version of ISO 9001:2015, while adding requirements relating to quality and safety. Major aerospace manufacturers and suppliers worldwide require compliance and/or registration to AS/EN 9100 as a condition of doing business with them.Mark Badge, Quality Manager, added: “Our employees in Leicester have worked hard over the last four years to construct the foundation for this achievement, transitioning to 9001:2015 and 14001:2015, and the latest rail standards so this really is a testament to their commitment.”
As an aerospace quality Management System (QMS) standard based on ISO 9001:2015, AS9100 Rev D contains additional requirements specific to the aerospace industry. By integrating QMS requirements into a company’s business processes, the Standard makes it possible to identify manufacturers which produce high-quality goods for the aerospace sector, both efficiently and consistently.
Question. Imagine. Design and Solve. Our Aerospace team are here to help solve your next challenge.