cd1

Trelleborg announces launch of PneuTrac – a new generation of agricultural tires

Trelleborg announces launch of PneuTrac – a new generation of agricultural tires
Trelleborg announces the launch of its latest innovation – the PneuTrac, a solution that combines the advantages both of radial argicultural tires and tracks.

Vineyards and orchards form two critical parts of agricultural production and both face unique challenges, notably in root protection and terrain. Vineyards often incorporate steep terrain and along with orchards, typically have narrow row operations with small spaces between vines or trees. Tracked applications can often be too wide to pass between rows with a comfortable margin for error.

Lorenzo Ciferri, VP Marketing & Communications at Trelleborg, commented: “PneuTrac delivers unbeatable performance on both steep slopes and muddy terrain, reducing downtime to zero in demanding conditions. PneuTrac combines the advantages of a radial agricultural tire in terms of fuel efficiency, comfort and handling, with the footprint and traction benefits of a track..”

PneuTrac contains the best-in-class features of Trelleborg agricultural tires along with a new sidewall utilizing CupWheel Technology by Galileo Wheel Ltd. The innovative “Omega” design of the sidewall helps the carcass to sustain load, simultaneously providing flexibility and an extra-wide footprint, resulting in very low soil compaction.

This new design allows the tread to work at 100% of its potential efficiency. The Progressive Traction technology on the tread itself enhances traction whilst the inter-lug terraces improve the self-cleaning capability of the tire. The wide lug bases combined with a robust shoulder feature, increase lateral stability, especially on slopes.

Ciferri, continued: “When designing the PneuTrac we focused on the specialist requirements of key producers. For example, the roots of vines are incredibly precious and susceptible to damage. As with conventional agriculture, the top soil needs to be protected and machine slippage could easily be a disaster for both the soil and roots.

“We firmly believe that PneuTrac is a game changing innovation and that it again demonstrates our commitment to sustainable farming, helping to protect some of our most valuable agricultural assets.”

PneuTrac will be on display at Agritechnica 2017, November 12 to 18 in Hannover, Germany. Further information will be available at Trelleborg’s Agritechnica Press Conference on Monday November 13th 2017.