Trelleborg Launches new Pit Stop Line for 25% increased tire life
Incorporating an orange line which is embedded into the tyre, the indictor is visible on the tyre wall and is designed to reveal itself across the surface of the tyre when the rubber has reached the end of its lifetime.
Trelleborg Business Unit President, Jean-Paul Mindermann, commented: “Tyres are often replaced with up to 25% of their life remaining simply because people are unaware that tread depth has nothing to do with the life of a solid tyre. Not only does this misconception cause a great amount of wastage, but it also costs companies thousands of euros every year through unnecessary tyre replacement and machine downtime.
“Now with the help of Trelleborg’s latest breakthrough, users can be alerted when the tyre has around 100 hours of life left, so that they can plan the replacement and eliminate those unnecessary costs.”
The new Pit Stop Line completely encompasses the European Tyre and Rim Technical Organization (ETRTO) Manual recommendations on tyre safety and enables 100% accurate tyre safety checks; a huge first for the industry.
Delivering more than just better value for spend; its sophisticated design will help improve machine uptime and service planning. With the Pit Stop Line appearing 100 hours or five to 15 working days before the tyre needs replacing, operators are able to plan their tyre changes in advance, totally eradicating unplanned downtime.
Pit Stop Line also offers a strong environmental benefit, enabling a dramatic reduction in waste, raw material as well as the carbon footprint associated with packaging and transportation. Replacing tyres less often means a reduced environmental impact.
Mindermann continued: “The Pit Stop Line has the potential to have a transformational effect on forklift operations, helping to minimize downtime, tyre waste and whole life costs – a true innovation. Tyre waste is now a thing of the past.”
For additional information regarding this product, please visit our website at www.trelleborg.com/en/wheels.