A smoother quieter journey

Aerial-view-of-car-in-woods
A smoother, quieter journey
If you thought electric cars were silent, think again. Electric drivelines are certainly quieter than internal combustion engines, but they have their own noise and vibration issues. Thankfully, new technology from Trelleborg helps ensure a smoother, quieter journey.

When electric cars were invented, many people thought the noisy world of the internal combustion engine would soon be history. But while electric and hybrid electric cars are quieter, it doesn’t mean they’re silent.

Electric drivelines have their own range of noise, vibration and harshness issues. And the noise of a typical combustion engine is no longer there to mask other structure-borne noises from the likes of the gearbox housing. But  there’s also another culprit.

“Power inverters are one of the main contributing sources of noise in the electric vehicles’ driveline,” says Reine Axelsson, Product Manager for Laminates for damping solutions within Trelleborg Sealing Solutions.

This worries automotive industry Original Equipment Manufacturers (OEMs) and their component suppliers. E-mobility is a fast-growing market, and the last thing they need is a noisy car that puts off potential consumers.

When a component supplier had a power inverter noise issue, it approached Trelleborg for help.

Trelleborg’s solution is based on the same basic technology used for brake shims. It’s called Applied Damping Material (ADM), a constrained layer damping material that consists of metal layers that have been vulcanized together with rubber to produce a strong and durable laminate. Together, the polymers, rubber and adhesive are an excellent material to absorb mechanical energy and the vibrations that radiate noise.

It works on all sorts of vibrating structures in automotive drivelines, but Trelleborg has come up with a new variant of ADM for the power inverter issue. 

“We’ve developed a completely new material for inverters because they make a wider range of noise,” says Arvid Norberg, Director of Sales and Marketing for damping solutions at Trelleborg. “By combining a different thickness of metal with different types of polymer thickness you can have a higher level of damping at a wider noise  frequency and temperature.”

The exact material composition is secret. Suffice it to say the polymers are based on nitryl butadiene rubber (NBR), and the adhesive is typically an acrylic, though other materials can also be involved.

But it’s a challenging development process because electrical engines and drives have even tougher cleanliness standards than combustion engines.

“The most critical thing is that there are no loose metallic particles past a certain size, as these can get into the engine or even the electronics and cause a short circuit,” Axelsson says. “We are asked to control the level of particles on the parts we supply.” 

Norberg adds, “We’re talking about tenths of millimeters that are often invisible to the naked eye.”

With the growth of e-mobility, Norberg believes ADM has significant market potential. It underlines the decision of Trelleborg Sealing Solutions several years ago to diversify from brakes and solidify its marketleading position in damping solutions. The team working in this area is growing too.

“We are at the forefront of the market, and we see e-mobility as being very important in the years ahead,” says Norberg.

So how will the technology develop?

“We’re using more lightweight materials wherever possible,” says Axelsson. “Our focus is noise and vibration, but we are also looking to see how we can respond to other new requirements that come from our customers. There are also new workplace directives on noise from the European Union to consider. The health and safety requirements regarding noise and vibration are only getting tougher, but that’s good for us as we’re regarded as the leading developer of brake and damping products.”

With the possibility of this technology being used in other industries such as consumer electronics, it’s clear that ADM has enormous potential, keeping Trelleborg ahead of the competition.




For more information
, please go to:
https://www.rubore.com/en


This is an article has been reproduced from Trelleborg's T-Time magazine. To download the latest edition, go to: www.trelleborg.com/t-time 


Press Service: This article is available in eight languages. Media are welcome to use this article in their own publications. To download the article and pictures in any language go to https://bamboo-contentpartner.com/. If you reproduce information from this release, please give contact details as: www.trelleborg.com.