Cable glands, grommets and cable entry covers

Electronic components are sensitive and require protection. To ensure uninterrupted mobile phone service and the continuous flow of electricity, these types of devices need to be protected from particles and moisture, as well as from electromagnetic interference.

Multigates, grommets and cable entry coversThis is particularly true if an electronic or electrical device, such as a telecom base station or an electrical switchgear cabinet, is to be installed outdoors where a number of wires and cables lead to it.

Trelleborg offers various types of connector shields, cable entry covers, cable glands, grommets and seals to solve this problem.

Fire-retardant and conductive thermoplastic elastomers and silicones have been developed to withstand harsh winters, bright sunshine and heavy rain.


For more information, please visit:
www.trelleborg.com/Industrial-Products



Senast uppdaterad 2012-04-18 |  Skriv ut sidan Skriv ut sidan |  Skicka sidan Skicka sidan   Facebook   Twitter
Skicka sidanx


Mottagarens e-post address


Din e-post address


Rubrik


Ditt meddelande





© Trelleborg AB (publ), P.O. Box 153, SE-231 22 Trelleborg, tel: +46 410 670 00