Structural Bearings

Structural elastomeric bearings need to transmit loads and accommodate horizontal movements and rotations around each axis that can occur between two structures. Design analyses will determine the scale of the forces and deformations.

In order to change their field of application the elastomeric bearings can be combined with complementary bearing devices, such as a restrain system or a sliding system. The restrain type prevents movements in all horizontal directions. Sliding systems, with or without guides, allow movements bigger than the shear capacity in plane surfaces.

Since 2005 the European standard EN 1337-3 has applied to elastomeric bearings for architectural and civil-engineering applications. Besides the functional requirements, the standard describes the design rules, the material properties, the production tolerances and the acceptance tests. Trelleborg designs and manufactures elastomeric bearings in accordance with this standard.

Experience shows that, under normal circumstances and with regular maintenance, Trelleborg’s structural bearings can function for decades.

For more information, please visit:

www.trelleborg.com/infrastructure

 

Contacts


Fabrik Fabrik    Försäljningskontor Försäljningskontor

Australia

 Manufacturing Plants & Logistic Centers Sales Office
Trelleborg Engineered Systems Australia Pty Ltd
515 Zillmere Rd.
AU-Zillmere, QLD 4034
Australia
tel: +61 7 3866 7444
fax: +61 7 3263 4912
www.trelleborg.com.au




Netherlands, the

 Manufacturing Plants & Logistic Centers Sales Office
Trelleborg Ridderkerk BV
(Trelleborg Bakker)
Postbus 4007
Verlengde Kerkweg 15
NL-2980 GA Ridderkerk
The Netherlands
tel: +31 180 49 55 55
fax: +31 180 43 07 20
www.trelleborg.com/infrastructure




Singapore

 Manufacturing Plants & Logistic Centers Sales Office
Trelleborg Singapore Pte Ltd
4 Jalan Pesawat
SG-Singapore 619362
Singapore
tel: +65 6265 0955
fax: +65 6265 9853
www.trelleborg.com/hercules




Spain

 Manufacturing Plants & Logistic Centers Sales Office
Trelleborg Izarra S.A.U.
C/San Vicente, 25
ES-01440 Izarra (Alava)
Spain
tel: +34 945 43 70 90
fax: +34 945 43 70 50


Senast uppdaterad 2011-11-24 |  Skriv ut sidan Skriv ut sidan |  Skicka sidan Skicka sidan   Facebook   Twitter
Skicka sidanx


Mottagarens e-post address


Din e-post address


Rubrik


Ditt meddelande





© Trelleborg AB (publ), P.O. Box 153, SE-231 22 Trelleborg, tel: +46 410 670 00
uiqt|wB|yz5qvnwH|zmttmjwzo5kwu|yz5qvnwH|zmttmjwzo5kwuuiqt|wBzqllmzsmzsH|zmttmjwzo5kwuzqllmzsmzsH|zmttmjwzo5kwuuiqt|wBpmzk}tm{H|zmttmjwzo5kwupmzk}tm{H|zmttmjwzo5kwuuiqt|wBq%zizziH|zmttmjwzo5kwuq%zizziH|zmttmjwzo5kwu