Vibration Isolation Bearings

To prevent damage from earthquakes our bearings are for example used in at the 911 Emergency Operations Centre in San Francisco, USA.
The acoustic bearings are used to prevent noise transmission and vibration when a building is close or even built over a subway or trainline. Our reference list is extensive and includes prestiguous objects such as the Disney Concert Hall in Los Angeles, USA and the Symphony Hall in Birmingham, UK.
Trelleborg designs and manufactures ANDRE elastomeric steel composite bearings to support and isolate a variety of buildings.
For more information, please visit:www.trelleborg.com/infrastructure
Fabrik
Försäljningskontor