Calendered Product Line of Fairprene Inc Available at Trelleborg

Calendered Product Line of Fairprene Inc®.: Available at Trelleborg
RUTHERFORDTON, NC – March, 15, 2018: Trelleborg’s engineered coated fabrics operations boasts the industry’s most comprehensive product offering of polymer-coated gasketing materials, including products using the original product specifications and formulations of the calendered product line of Fairprene, Inc.® which have been specified in thousands of end-use applications across a multitude of market segments.

The original Fairprene® calendered product line acquired by Trelleborg is manufactured in Trelleborg’s facility in Rutherfordton, North Carolina. These products, combined with more recent advancements in materials and processes, represent Trelleborg’s commitment to providing its customers with solutions proven by decades of success in the field as well as new and ever-evolving capabilities. Trelleborg’s goal is to provide innovative solutions that accelerate performance for its customers in a sustainable way.

To find out more about Trelleborg’s unrivalled polymer engineering expertise and application processes visit them at the Gasketing/Coverting Expo from March 19 to 21 in Orlando, Florida, or stop by booth 1821 at Techtextil North America, May 22 to 24 in Atlanta, Georgia.

You can also connect with Trelleborg’s engineered coated fabrics operation on LinkedIn to join the conversation, and keep up with their latest innovations that are positively impacting the world.

Fairprene® is a registered trademark of Alpha Engineered Composites, LLC.