Bend Control Solutions - Trelleborg Offshore

Bend Control Solutions

Where any flexible tubular connects to a structure, normal movement during operation or forces incurred during installation can cause catastrophic failure of the tubular at the termination point. The failure mode can be through collapse, rupture of internal lines or even rupture of the external layers leading to escape of the contents to the environment. This can be caused through fatigue damage over time. Our Bend control solutions reduce this damage.

8products

Showing 0 of 8 products

Load More

Learn more about how we solve your challenges

bend control solutions 
Subsea - Bend Control

Deepwater Performance in Brazil


The Petrobras P-58 FPSO, which operates on the Baleia Azul field in the Parque das Baleias area, north of the Campos Basin in Brazil, is moored 48 miles / 78 km offshore in a water depth of 4,593 feet / 1,400 meters, and is expected to last 25 years. Oil production, which commenced in March 2014, comes from 19 satellite wells connected individually to the unit.
bend control solutions
Renewables - Bend Control

Protected performance for the world’s largest floating windfarm


This floating wind turbine project is truly unique. The project, which is being headed up by The Ministry of Economy, Trade and Industry in Japan, will be the world’s largest floating wind farm once complete. Located 16 kilometers off the coast of the Fukushima Daiichi nuclear power plant, it is being developed in wake of the devastating earthquake and tsunami which hit Fukushima in March 2011.
Trelleborg World Map

Our skilled staff will contact you within one business day.

*
*
*
*
*
*
Seismic
Surface
Drilling
Topside
Downhole
Renewables
Subsea
Other
*