Contact Us
Trelleborg Offshore have offices and facilities in Europe and North America - for further contact details please click on the link below:
Office and Facilities
Trelleborg Offshore have a worldwide network of agents and distributors - for further contact details please click on the link below:
Agents and Distributors






Testing

Testing
We have a modern and well equipped QA/QC laboratory which allows most material testing (tensile, compressive etc) to be conducted in-house

Factory acceptance testing of bending restrictors can be divided into three main categories:
 
Materials testing
 
Fit-up, assembly testing
 
Load testing



Materials Testing
 
Stringent quality control checks are carried out on all batches of polyurethane material used in the manufacture of Bending Restrictors. This includes both good-inwards and in-process checks to ensure that only raw materials with the correct material properties are put into production and that these properties remain consistent throughout the manufacturing process.
 
We have a modern and well equipped QA/QC laboratory which allows most material testing (tensile, compressive etc) to be conducted in-house. Alternatively if Third Party Approval test results are required, we have free access to a local NAMAS Approved Test House.
 
Fit-Up and Assembly Testing
 
Generally when a client opens the packing case for the first time, he will be offshore on an installation vessel. It is therefore vital that in order to prevent expensive delays, all the components of the Bending Restrictor fit-up and assemble together as requested.
 
As a matter of routine, the Bending Restrictor elements will be fully assembled in a string using the correct fasteners prior to release for despatch from us.
 
In addition, the elements will be assembled onto the particular interface steelwork component, which in turn will be fitted up to either the real or a mock-up of the rigid interface structure.
 
Load Testing
 
To ensure that the Bending Restrictor has a suitable load capacity, many clients specifiy that a load test is undertaken, two types of load test can be conducted:
 
  • Proof load testing
  • Destructive load testing

 

With the proof load test, a fully assembled string of elements is subjected to the calculated maximum in service loading. The load is held for a defined time period and the restrictor is then examined for any signs of damage.

If a destructive load test is specified, the Restrictor is first proof load tested then the load is increased until failure of one or more of the elements occurs. The failure load is recorded and compared to the load anticipated by calculation methods.

 
Last updated 2007-09-10 |  Print this page Print this page |  E-mail this page E-mail this page   Facebook   Twitter
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message