Trelleborg Unveils Rotary Shaft Seal Designed to Boost the Motorsport Industry

Rotary shaft seal

Trelleborg Unveils Rotary Shaft Seal Designed to Boost the Motorsport Industry

Trelleborg Sealing Solutions has launched an innovative rotary shaft seal which provides "superior execution" and will "out-perform" other products on the market. The Turcon® Varilip® PDR rotary shaft seal has fast become the chosen product by several high profile motorsport clients who know it will maximise results and keep their teams winning.

Carefully developed to extend the boundaries imposed by elastomer radial shaft seals, the Turcon® Varilip® PDR rotary shaft seal utilizes advanced materials and design techniques to provide optimum sealing performance for motorsport applications. It is characterized by low friction stick-slip-free running, reducing temperature generation and permitting higher peripheral speeds. 

Andrew Longdon, UK Technical Manager at Trelleborg Sealing Solutions, said: "We have become the leading producers of lightweight, friction-reducing rotary shaft seals which are successfully used on Formula One and IndyCar racing platforms. Rotary seal torque and power consumption varies greatly with seal designs and material, which is why it has become so important to identify seal configurations that achieve the best possible performance for racing requirements. 

"The design for the Turcon® Varilip® PDR rotary shaft provides a superior sealing solutions which retains a compact seal evelope. It is accepted that standard elastomeric rotary shaft seals have a limited application range, which is why we know the Turcon® Varilip® PDR rotary shaft seal will out perform other products on the market every time." 

What makes the seal truly unique is the fact it is constructed from only two parts - a precision manufactured metal body and a mechanically retained Turcon® 
sealing element. Unlike seals with pressed metal cases, a gasket is not required to provide sealing between the lip and casing. This is provided by the mechanical retention of the lip, improving the chemical resistance and temperature range of the sealing system. 

The option of an integrated end plate for Turcon® Varilip® PDR rotary shaft seal can also allow end users to optimize their hardware design to minimize envelope and part count. 

In addition, the Turcon® Varilip® PDR rotary shaft seal us available with a hydrodynamic feature on the Turcon® sealing lip which provides a positive displacement of fluid as result of the shaft rotation to give improved sealing in applications where the shaft only rotates in a single direction. The feature also increases the flexibility of the lip, allowing a wider contact area between the Turcon® lip and the shaft, helping to reduce shaft load and associated wear and temperature generation. 

As well, like all Turcon® Varilip® PDR seals, the rotary shaft seal is capable of outstanding high and low temperature performance compared to elastomeric materials.

Unlike other PTFE lip seals, Trelleborg’s Turcon® Varilip® PDR seal is not limited in its temperature performance by the presence of an elastomer gasket. This gives it excellent temperature range capability. It also has an exceptional resistance to oil additives and biofuels, which can have an adverse effect on many elastomers. Using Turcon® shaft seals therefore allows the increased use of additives and gives a longer oil service life.

For more information, please go to: 

Press Service:
This press release is available for download in English. If you reproduce information from this release please give contact details as: