Trelleborg Aims At Eliminating Risk From Docking & Mooring

Trelleborg Aims At Eliminating Risk From Docking & Mooring

Trelleborg’s marine systems operation has launched a new whitepaper and on-demand webinar outlining design and compliance requirements in docking & mooring equipment, and a new best practice approach to specification.

Quick Release Hooks
The whitepaper, entitled ‘The Quest for Quality’, examines the relationship between cost and quality, explaining why low-cost equipment could prove costly for port owners and operators in the long term.

Hani William, Sales and Marketing Manager at Trelleborg’s marine systems operation, said: “The mooring operation is high risk. The UK P&I Club reports that in the UK in the last 20 years, 58% of injuries occurred during mooring and 26% were due to equipment failure. The Australian Maritime Safety Authority (AMSA) found that of 227 reported incidents between 2010 and 2014, 62% were related to design shortfalls or equipment failures, and 51% of the identified design and equipment safety factors were the result of a parted mooring line.

“Clearly, poorly designed, poorly considered or low-quality products ultimately risk the safety of personnel, the efficiency of operations and increase the total cost of ownership.”

Selecting docking and mooring systems can be a challenge. There are many variables to consider: design specification, safety features, installation method and more. In the webinar, William explores the best practice methodologies to which suppliers must adhere to ensure docking and mooring solutions are fit for purpose.

This article is also published on:
Marine Insight

Similar article:
Port Strategy

To read the whitepaper, click here. For the webinar, click here.