Trelleborg to Kick-start 2018 LNG Ship-Shore Interface Conference

Trelleborg to Kick-start 2018 LNG Ship-Shore Interface Conference

22-23 November 2018 | Venue: London, UK

As Platinum Sponsor, Trelleborg Marine Systems will deliver the welcoming address at The LNG Ship/Shore Interface Conference, which will be held in London, UK, 22-23 November 2018.

The LNG Ship/Shore Interface Conference will bring together Europe’s LNG transportation supply chain to discuss ship and terminal operations at the jetty, offshore and bunker station. At the conference, Dave Pendleton, Trelleborg Marine Systems' Managing Director, will deliver the welcoming address and will discuss the importance of businesses investment in innovation, and the critical role that the implementation of innovative solutions plays in the development of global markets. Steve Ward, Trelleborg Marine Systems' Technical Sales Manager will also provide a detailed look at a real-life case study in LNG bunkering, discussing the challenges met and the lessons learned.

Trelleborg will exhibit its Universal Safety Link (USL), an innovative product that takes the company’s expertise in large-scale LNG transfer applications, develops it and applies it to provide an optimized product for the burgeoning and diverse small and mid-scale LNG sectors. Delegates will also be able to learn about Trelleborg’s Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for over 20 years.

LNG Ship/Shore Interface Conference logo