Case Keeping Greenhouses Green - Trelleborg Fluid Handling Solutions - Trelleborg AB

Keeping Greenhouses Green

A greenhouse hose is a critical – and problematic – element for the agricultural industry in the Netherlands. Trelleborg helped to develop a flexible hose solution that answered the challenge.

The Netherlands is a leading producer of fruit and vegetables, accounting for a quarter of Europe’s vegetable exports. Its diverse agricultural sector includes arable, dairy and livestock farming, garden plants, bulbs and flowers, as well as a highly developed greenhouse industry growing tomatoes, peppers, cucumbers and eggplants. 

The Netherlands leads the world in both greenhouse cultivation and the technologies necessary to maintain optimum growing conditions and output. In 2010, the total area for vegetables under glass was 12,000 acres, producing 3,390 million pounds of exported fresh greenhouse vegetables. 

There are three main types of greenhouse: “cold,” using the sun as a heat source; “frost,” in which a low-power heating system maintains a small temperature difference between outside and inside temperatures; and “warm.” This last condition is the greenhouse environment typically used by Dutch growers, deploying new technologies and methods in robotics, water and waste recycling, lighting and energy efficiency. 

The main Dutch system of greenhouse heating uses an overhead suspended hot water steel pipe network interconnected with flexible hoses that can be raised or lowered to make room for equipment and machinery used inside the greenhouses and to deliver heat to the optimum position of growth for a plant. In the 1980s the hoses used in these systems were constantly giving growers problems, one of the most serious being the release of toxic gases from the hose material that could kill crops. 

Olivier Libes, Marketing and Product Development Manager for fluid handling solutions at Trelleborg explains: “In response to serious problems with the hoses being used in many greenhouses, we developed a dedicated hose, Kledam, which has become the de facto standard. We worked in collaboration with Dutch greenhouse builders and installers, with substantial input from heating technicians and agricultural engineers, to produce a hose that has exceptional resistance to wearing, aging and weathering. It’s flexible and remarkably reliable, with zero emissions of toxic gases.” 

Each year the Kledam hose undergoes and passes rigorous testing by the Wageningen University Research Centre, the most authoritative agrifood and nutrition research facility in Europe. It’s a testimony to Trelleborg’s commitment to solutions of the highest quality. 

Andre Persoon is the heating engineer at Certhon, one of Holland’s leading greenhouse design, construction and installation companies. “We supply greenhouses and installations worldwide and have a reputation for excellence in greenhouse horticulture solutions. It’s vital for us to know that components in our systems are the best. There are three critical criteria for the hoses that we use to connect the steel heating loops: The hose material cannot give off any toxic gases, it needs to be flexible and strong to cope with the variations in height of the heating loops, and it must seal cleanly and tightly over the connectors. The Kledam hose system fulfills all these requirements and has never let us down.”

Equally enthusiastic is Arjen Bonnema, director of Arbon Agenturen BV, sole distributor for the Kledam hose in the Netherlands. “The hose is made of a special EPDM [ethylene propylene diene monomer] compound developed by Trelleborg for the inner tube, reinforced with synthetic textile material,” he says. “It’s able to withstand temperature ranges of -30° C to +95° C and performs superbly. It has rope-like flexibility, the strength of steel, does not leak, and despite wide variations in environmental conditions is very durable. The Kledam hose has become the benchmark for products in this field, and Trelleborg is the undisputed market leader.” 

Trelleborg offers solutions to the food, chemical and petrochemical, construction, environmental and agribusiness industries.

Facts Certhon

In 2011, two leading companies in greenhouse horticulture, Wilk van der Sande (technical installations) and Bosch Inveka (greenhouse construction), joined under a new group name: Certhon. Certhon is a market leader in high-tech integrated horticultural solutions, supplying greenhouses and technical installations worldwide. One of its most recent projects is the Dube TradePort Agrizone, South Africa’s largest greenhouse project, covering some 40 acres.